CfdAutoRefinementConstraintCollection Class¶
-
class
NXOpen.CAE.
CfdAutoRefinementConstraintCollection
¶ Bases:
object
Provides methods for managing automatic refinement constraints:py:class:CAE.CfdAutoRefinementConstraint in a fem part
To obtain an instance of this class, refer to
NXOpen.CAE.BaseFEModel
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
CloneConstraint | Clones an automatic refinement constraint |
CreateBuilder | Creates an automatic refinement constraint builder |
DeleteConstraint | Deletes an automatic refinement constraint |
Find | Finds the CAE.CfdAutoRefinementConstraint with the given identifier as recorded in a journal |
FindObject | Finds the CAE.CfdAutoRefinementConstraint with the given identifier as recorded in a journal |
Method Detail¶
CloneConstraint¶
-
CfdAutoRefinementConstraintCollection.
CloneConstraint
¶ Clones an automatic refinement constraint
Signature
CloneConstraint(source)
Parameters: source ( NXOpen.CAE.CfdAutoRefinementConstraint
) – Source constraintReturns: Cloned constraint Return type: NXOpen.CAE.CfdAutoRefinementConstraint
New in version NX11.0.0.
License requirements: nx_adv_fld_mod_solv (“NX Advanced Fluid Modeling - Full”) OR sc_acou_meshing (” SC Acoustic Meshing”)
CreateBuilder¶
-
CfdAutoRefinementConstraintCollection.
CreateBuilder
¶ Creates an automatic refinement constraint builder
Signature
CreateBuilder(recipe)
Parameters: recipe ( NXOpen.TaggedObject
) –CfdAutoRefinementConstraint
to be edited, if None orFluidDomainRecipe
then create a new oneReturns: the created builder Return type: NXOpen.CAE.CfdAutoRefinementConstraintBuilder
New in version NX11.0.0.
License requirements: nx_adv_fld_mod_solv (“NX Advanced Fluid Modeling - Full”) OR sc_acou_meshing (” SC Acoustic Meshing”)
DeleteConstraint¶
-
CfdAutoRefinementConstraintCollection.
DeleteConstraint
¶ Deletes an automatic refinement constraint
Signature
DeleteConstraint(constraint)
Parameters: constraint ( NXOpen.CAE.CfdAutoRefinementConstraint
) – The constraint to be deletedNew in version NX11.0.0.
License requirements: nx_adv_fld_mod_solv (“NX Advanced Fluid Modeling - Full”) OR sc_acou_meshing (” SC Acoustic Meshing”)
Find¶
-
CfdAutoRefinementConstraintCollection.
Find
¶ Finds the
CAE.CfdAutoRefinementConstraint
with the given identifier as recorded in a journalSignature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – constraint identifier Returns: constraint with this identifier Return type: NXOpen.CAE.CfdAutoRefinementConstraint
New in version NX11.0.0.
License requirements: None.
FindObject¶
-
CfdAutoRefinementConstraintCollection.
FindObject
¶ Finds the
CAE.CfdAutoRefinementConstraint
with the given identifier as recorded in a journalSignature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – constraint identifier Returns: constraint with this identifier Return type: NXOpen.CAE.CfdAutoRefinementConstraint
New in version NX11.0.0.
License requirements: None.