BoltCollection Class¶
-
class
NXOpen.CAE.
BoltCollection
¶ Bases:
object
Provides method for creating builder for bolt operation commands in a fem/afem part
To obtain an instance of this class, refer to
NXOpen.CAE.BaseFEModel
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateBoltBuilder | Creates a builder for Bolt Command |
FindObject | Finds the NXOpen.CAE.Bolt with the given identifier as recorded in a journal. |
Method Detail¶
CreateBoltBuilder¶
-
BoltCollection.
CreateBoltBuilder
¶ Creates a builder for Bolt Command
Signature
CreateBoltBuilder(bolt)
Parameters: bolt ( NXOpen.CAE.Bolt
) –NXOpen.CAE.Bolt
to be edited. if None then create a new oneReturns: Return type: NXOpen.CAE.BoltBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
FindObject¶
-
BoltCollection.
FindObject
¶ Finds the
NXOpen.CAE.Bolt
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Bolt name Returns: Bolt for given identifier Return type: NXOpen.CAE.Bolt
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)