Folder Class¶
-
class
NXOpen.CAE.Connections.
Folder
¶ Bases:
NXOpen.NXObject
The Folder class offers a way to create a hierarchy of connections and sub-folders
To obtain an instance of this object use the add_folder creator in a parent folder or access connection root folder from
CAE.IFEModel
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Parent | Returns the parent folder |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
ConnectionUtils | Returns a CAE.Connections.Utils instance |
Methods¶
Method | Description |
---|---|
AddFolder | Add a subfolder to this folder. |
CreateAttributeIterator | Create an attribute iterator |
CreateConnection | Create a CAE.Connections.IConnection in this folder of the specified type with the specified name |
CreateFolder | Creates a CAE.Connections.Folder in this folder with the specified name |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAllConnections | Get all the connections under this folder and its descendant folders |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetChildFolders | Get the child folders |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetConnections | Get the connections |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
ImportConnectionsFromMcf | Create CAE.Connections.IConnection connections in the current CAE.Connections.Folder using connection data imported from a MCF file. |
ImportSpotWeldFromWcd | Create CAE.Connections.SpotWeld connections in the current CAE.Connections.Folder using connection data imported from a WCD file. |
MoveConnectionToThisFolder | Add a connection to this folder. |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsOccurrence¶
-
Folder.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Folder.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Folder.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Folder.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Folder.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Parent¶
-
Folder.
Parent
¶ Returns the parent folder
-------------------------------------
Getter Method
Signature
Parent
Returns: parent folder Return type: NXOpen.CAE.Connections.Folder
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Prototype¶
-
Folder.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
ConnectionUtils¶
-
Folder.
ConnectionUtils
¶ Returns a
CAE.Connections.Utils
instanceSignature
ConnectionUtils
New in version NX12.0.0.
Returns: Return type: NXOpen.CAE.Connections.Utils
Method Detail¶
AddFolder¶
-
Folder.
AddFolder
¶ Add a subfolder to this folder.
The subfolder is moved if found in other folder.
Signature
AddFolder(subfolder)
Parameters: subfolder ( NXOpen.CAE.Connections.Folder
) – the added folderNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateConnection¶
-
Folder.
CreateConnection
¶ Create a
CAE.Connections.IConnection
in this folder of the specified type with the specified nameSignature
CreateConnection(type, name)
Parameters: - type (
NXOpen.CAE.Connections.ConnectionType
) – - name (str) – name of the connection
Returns: the created connection
Return type: New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- type (
CreateFolder¶
-
Folder.
CreateFolder
¶ Creates a
CAE.Connections.Folder
in this folder with the specified nameSignature
CreateFolder(name)
Parameters: name (str) – Name that the created folder should have Returns: the created CAE.Connections.Folder
Return type: NXOpen.CAE.Connections.Folder
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
FindObject¶
-
Folder.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAllConnections¶
-
Folder.
GetAllConnections
¶ Get all the connections under this folder and its descendant folders
Signature
GetAllConnections()
Returns: all connections under this folder and its descendants Return type: list of NXOpen.CAE.Connections.IConnection
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetChildFolders¶
-
Folder.
GetChildFolders
¶ Get the child folders
Signature
GetChildFolders()
Returns: child folders Return type: list of NXOpen.CAE.Connections.Folder
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetConnections¶
-
Folder.
GetConnections
¶ Get the connections
Signature
GetConnections()
Returns: connections found in folder Return type: list of NXOpen.CAE.Connections.IConnection
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ImportConnectionsFromMcf¶
-
Folder.
ImportConnectionsFromMcf
¶ Create
CAE.Connections.IConnection
connections in the currentCAE.Connections.Folder
using connection data imported from a MCF file.Signature
ImportConnectionsFromMcf(file, inputFileUnit)
Parameters: - file (str) – name of the import file
- inputFileUnit (
NXOpen.Unit
) – the length unit used in the input file
Returns: the created connections
Return type: New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ImportSpotWeldFromWcd¶
-
Folder.
ImportSpotWeldFromWcd
¶ Create
CAE.Connections.SpotWeld
connections in the currentCAE.Connections.Folder
using connection data imported from a WCD file.Signature
ImportSpotWeldFromWcd(file, inputFileUnit)
Parameters: - file (str) – name of the import file
- inputFileUnit (
NXOpen.Unit
) – the length unit used in the input file
Returns: the created connections
Return type: list of
NXOpen.CAE.Connections.SpotWeld
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MoveConnectionToThisFolder¶
-
Folder.
MoveConnectionToThisFolder
¶ Add a connection to this folder.
The connection is removed from previous parent folder.
Signature
MoveConnectionToThisFolder(connection)
Parameters: connection ( NXOpen.CAE.Connections.IConnection
) – the connection that is movedNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Print¶
-
Folder.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
Folder.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.