ConnectionType Enumeration¶
-
class
NXOpen.CAE.Connections.
ConnectionType
¶ Bases:
object
Connection type Enum Members
Enum Member Enum Member Description SpotWeld SpotWeld Adhesive Adhesive Bolt Bolt Spring Spring Rigid Rigid Bushing Bushing Damper Damper Kinematic Kinematic SeamWeld Seam Weld Sealing Sealing -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-