BeamSectionCollection Class¶
-
class
NXOpen.CAE.
BeamSectionCollection
¶ Bases:
object
Represents the collection of all
NXOpen.CAE.BeamSection
in a fem partTo obtain an instance of this class, refer to
NXOpen.CAE.BaseFEModel
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CloneSection | Creates a copy of a beam cross section |
CopyAsGeneralGeometrySection | Copies a section to a new general geometry section |
CreateGeneralGeometryBeamSectionBuilder | Creates a general geometry section builder. |
CreateStandardBeamSectionBuilder | Creates a standard section builder |
CreateUserDefinedSolidBeamSectionBuilder | Creates a user-defined solid section builder. |
FindObject | Finds the NXOpen.CAE.BeamSection with the given identifier as recorded in a journal. |
Method Detail¶
CloneSection¶
-
BeamSectionCollection.
CloneSection
¶ Creates a copy of a beam cross section
Signature
CloneSection(sourceSection)
Parameters: sourceSection ( NXOpen.CAE.BeamSection
) – Section to be copiedReturns: Cloned section Return type: NXOpen.CAE.BeamSection
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CopyAsGeneralGeometrySection¶
-
BeamSectionCollection.
CopyAsGeneralGeometrySection
¶ Copies a section to a new general geometry section
Signature
CopyAsGeneralGeometrySection(sourceSection)
Parameters: sourceSection ( NXOpen.CAE.BeamSection
) – Section to be copiedReturns: Copied general geometry section Return type: NXOpen.CAE.GeneralGeometryBeamSection
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateGeneralGeometryBeamSectionBuilder¶
-
BeamSectionCollection.
CreateGeneralGeometryBeamSectionBuilder
¶ Creates a general geometry section builder.
Signature
CreateGeneralGeometryBeamSectionBuilder(section)
Parameters: section ( NXOpen.CAE.GeneralGeometryBeamSection
) –NXOpen.CAE.GeneralGeometryBeamSection
to be editedReturns: General geometry beam section builder Return type: NXOpen.CAE.GeneralGeometryBeamSectionBuilder
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateStandardBeamSectionBuilder¶
-
BeamSectionCollection.
CreateStandardBeamSectionBuilder
¶ Creates a standard section builder
Signature
CreateStandardBeamSectionBuilder(section)
Parameters: section ( NXOpen.CAE.StandardBeamSection
) –NXOpen.CAE.StandardBeamSection
to be editedReturns: Standard beam section builder Return type: NXOpen.CAE.StandardBeamSectionBuilder
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateUserDefinedSolidBeamSectionBuilder¶
-
BeamSectionCollection.
CreateUserDefinedSolidBeamSectionBuilder
¶ Creates a user-defined solid section builder.
Signature
CreateUserDefinedSolidBeamSectionBuilder(section)
Parameters: section ( NXOpen.CAE.UserDefinedSolidBeamSection
) –NXOpen.CAE.UserDefinedSolidBeamSection
to be editedReturns: User-defined solid beam section builder Return type: NXOpen.CAE.UserDefinedSolidBeamSectionBuilder
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
BeamSectionCollection.
FindObject
¶ Finds the
NXOpen.CAE.BeamSection
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Beam Section name Returns: Beam Section with this identifier Return type: NXOpen.CAE.BeamSection
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)