ScrapDesignBuilder Class¶
-
class
NXOpen.Tooling.
ScrapDesignBuilder
¶ Bases:
NXOpen.Builder
Represents a scrap design builder
To create a new instance of this class, use
NXOpen.Tooling.ScrapDesignCollection.CreateScrapDesignBuilder()
Default values.
Property Value AddonOperation Overlap ApplyColor 0 DefStationNum 1 DoubleA 0 DoubleAngle 0 DoubleB 0 DoubleH 0 DoubleR 0.2 EditMethod Split EditStationNum 1 MinRad 0.1 OvercutOperation NormalType OverlapWidth 0.1 PierceType Piercing ProcessFive 0 ProcessFour 0 ProcessOne 0 ProcessThree 0 ProcessTwo 0 RemoveFilter InferScrap ScrapPosition ProjectToStrip ScrapTol 0.01 ScrapTypeEnum Create New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AddonOperation | Returns or sets the add-on operation, which includes overlap, overcut, trimming and user defined |
ApplyColor | Returns or sets the toggle to determine whether the color will be used to all other scraps with the same shape |
AssignColor | Returns or sets the color for assigned scrap |
AttachEdge | Returns the edge that overlap will be attached |
AttachScrap | Returns the scrap that overlap will be attached |
BoundaryList | Returns the boundary list served for boundary line method |
ChangeColScrap | Returns the changing color of scrap |
CurveList | Returns the curve list served for boundary+sketch or close boundaries method |
DefStationNum | Returns or sets the defined station number, according to it scraps can be laid out automatically in strip |
DoubleA | Returns or sets the double A served as the parameter of overcut |
DoubleAngle | Returns or sets the double Angle served as the parameter of overcut |
DoubleB | Returns or sets the double B served as the parameter of overcut |
DoubleH | Returns or sets the double H served as the parameter of overcut |
DoubleR | Returns or sets the double R served as the parameter of overcut |
EditMethod | Returns or sets the edit method, which includes splitting, merging, applying minimum radius, changing station, deleting and updating |
EditStationNum | Returns or sets the station number to lay out in strip |
ExistScrap | Returns the existed scrap served for exist sheet body method |
HoleColor | Returns or sets the hole color |
MinRad | Returns or sets the minimum radius to blend sharp corners |
OvercutColor | Returns or sets the overcut color |
OvercutEdge | Returns the edge that overcut will be attached |
OvercutOperation | Returns or sets the overcut operation, which includes normal type, tangent type, circular type and rectangular type |
OverlapColor | Returns or sets the overlap color |
OverlapWidth | Returns or sets the overlap width |
PierceType | Returns or sets the piercing type, piercing or piloting |
PiercingColor | Returns or sets the piercing color |
PilotingColor | Returns or sets the piloting color |
ProcessFive | Returns or sets the process five |
ProcessFour | Returns or sets the process four |
ProcessOne | Returns or sets the process one |
ProcessThree | Returns or sets the process three |
ProcessTwo | Returns or sets the process two |
RemoveFilter | Returns or sets the removing filter |
ScrapMethod | Returns or sets the scrap method, which includes boundary+sketch, hole boundary, close curves, boundary lines and existed sheet body |
ScrapPosition | Returns or sets the scrap position |
ScrapTol | Returns or sets the scrap tolerance, when fail to create scrap in some cases, this value can be decreased to try again |
ScrapTypeEnum | Returns or sets the scrap type enum |
SecondScrap | Returns the second scrap to merge with the first one |
SplitCurve | Returns the splitting curve |
SplitScrap | Returns the scrap to be splitted or merged |
Tag | Returns the Tag for this object. |
TrimNum | Returns or sets the trimming number |
TrimmingColor | Returns or sets the trimming color |
UserAddonCurve | Returns the user defined add-on curve to create overlap+overcut |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOvercutPosition | Returns the overcut position, it determines where the overcut sketch will be constrained @return Indicates the position to constrain overcut sketch |
SetOvercutPosition | Sets the overcut position, it determines where the overcut sketch will be constrained |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ScrapDesignBuilderAddonType Enumeration | Specifies the add-on type |
ScrapDesignBuilderBody Enumeration | Specifies the operation type of scraps |
ScrapDesignBuilderDefScrapType Enumeration | Specifies the definition type of scraps |
ScrapDesignBuilderEditScrapType Enumeration | Specifies the edit type of scraps |
ScrapDesignBuilderOvercutType Enumeration | Specifies the over cut type, different type has different parameters |
ScrapDesignBuilderRemoveType Enumeration | Specifies the removing type as filter |
ScrapDesignBuilderScrapDefPosition Enumeration | Specifies the position method of scraps, projecting method is normally used |
ScrapDesignBuilderScrapDefType Enumeration | Specifies the creation type of scraps |
ScrapDesignBuilderTrimNumType Enumeration | Specifies the step of trimming process, the maximum is five |
Property Detail¶
AddonOperation¶
-
ScrapDesignBuilder.
AddonOperation
¶ Returns or sets the add-on operation, which includes overlap, overcut, trimming and user defined
-------------------------------------
Getter Method
Signature
AddonOperation()
Returns: Indicates the add-on operation Return type: NXOpen.Tooling.ScrapDesignBuilderAddonType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AddonOperation(addonOperation)
Parameters: addonOperation ( NXOpen.Tooling.ScrapDesignBuilderAddonType
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ApplyColor¶
-
ScrapDesignBuilder.
ApplyColor
¶ Returns or sets the toggle to determine whether the color will be used to all other scraps with the same shape
-------------------------------------
Getter Method
Signature
ApplyColor()
Returns: Indicates whether the color will be used to all other scraps Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplyColor(applyColor)
Parameters: applyColor (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
AssignColor¶
-
ScrapDesignBuilder.
AssignColor
¶ Returns or sets the color for assigned scrap
-------------------------------------
Getter Method
Signature
AssignColor()
Returns: Indicates the color of scraps Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssignColor(assignColor)
Parameters: assignColor (Id) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
AttachEdge¶
-
ScrapDesignBuilder.
AttachEdge
¶ Returns the edge that overlap will be attached
-------------------------------------
Getter Method
Signature
AttachEdge()
Returns: Return type: NXOpen.SelectEdgeList
New in version NX6.0.0.
License requirements: None.
AttachScrap¶
-
ScrapDesignBuilder.
AttachScrap
¶ Returns the scrap that overlap will be attached
-------------------------------------
Getter Method
Signature
AttachScrap()
Returns: Return type: NXOpen.SelectBody
New in version NX6.0.0.
License requirements: None.
BoundaryList¶
-
ScrapDesignBuilder.
BoundaryList
¶ Returns the boundary list served for boundary line method
-------------------------------------
Getter Method
Signature
BoundaryList()
Returns: Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: None.
ChangeColScrap¶
-
ScrapDesignBuilder.
ChangeColScrap
¶ Returns the changing color of scrap
-------------------------------------
Getter Method
Signature
ChangeColScrap()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
CurveList¶
-
ScrapDesignBuilder.
CurveList
¶ Returns the curve list served for boundary+sketch or close boundaries method
-------------------------------------
Getter Method
Signature
CurveList()
Returns: The curve list is to create scraps Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
DefStationNum¶
-
ScrapDesignBuilder.
DefStationNum
¶ Returns or sets the defined station number, according to it scraps can be laid out automatically in strip
-------------------------------------
Getter Method
Signature
DefStationNum()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefStationNum(defStationNum)
Parameters: defStationNum (int) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DoubleA¶
-
ScrapDesignBuilder.
DoubleA
¶ Returns or sets the double A served as the parameter of overcut
-------------------------------------
Getter Method
Signature
DoubleA()
Returns: Indicates the parameter A of overcut Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleA(doubleA)
Parameters: doubleA (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DoubleAngle¶
-
ScrapDesignBuilder.
DoubleAngle
¶ Returns or sets the double Angle served as the parameter of overcut
-------------------------------------
Getter Method
Signature
DoubleAngle()
Returns: Indicates the parameter Angle of overcut Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleAngle(doubleAngle)
Parameters: doubleAngle (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DoubleB¶
-
ScrapDesignBuilder.
DoubleB
¶ Returns or sets the double B served as the parameter of overcut
-------------------------------------
Getter Method
Signature
DoubleB()
Returns: Indicates the parameter B of overcut Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleB(doubleB)
Parameters: doubleB (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DoubleH¶
-
ScrapDesignBuilder.
DoubleH
¶ Returns or sets the double H served as the parameter of overcut
-------------------------------------
Getter Method
Signature
DoubleH()
Returns: Indicates the parameter H of overcut Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleH(doubleH)
Parameters: doubleH (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DoubleR¶
-
ScrapDesignBuilder.
DoubleR
¶ Returns or sets the double R served as the parameter of overcut
-------------------------------------
Getter Method
Signature
DoubleR()
Returns: Indicates the parameter R of overcut Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleR(doubleR)
Parameters: doubleR (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
EditMethod¶
-
ScrapDesignBuilder.
EditMethod
¶ Returns or sets the edit method, which includes splitting, merging, applying minimum radius, changing station, deleting and updating
-------------------------------------
Getter Method
Signature
EditMethod()
Returns: Indicates the edit method Return type: NXOpen.Tooling.ScrapDesignBuilderEditScrapType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EditMethod(editMethod)
Parameters: editMethod ( NXOpen.Tooling.ScrapDesignBuilderEditScrapType
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
EditStationNum¶
-
ScrapDesignBuilder.
EditStationNum
¶ Returns or sets the station number to lay out in strip
-------------------------------------
Getter Method
Signature
EditStationNum()
Returns: Indicates the station number of scraps Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EditStationNum(editStationNum)
Parameters: editStationNum (int) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ExistScrap¶
-
ScrapDesignBuilder.
ExistScrap
¶ Returns the existed scrap served for exist sheet body method
-------------------------------------
Getter Method
Signature
ExistScrap()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
HoleColor¶
-
ScrapDesignBuilder.
HoleColor
¶ Returns or sets the hole color
-------------------------------------
Getter Method
Signature
HoleColor()
Returns: Indicates the color of hole scraps Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HoleColor(holeColor)
Parameters: holeColor (Id) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
MinRad¶
-
ScrapDesignBuilder.
MinRad
¶ Returns or sets the minimum radius to blend sharp corners
-------------------------------------
Getter Method
Signature
MinRad()
Returns: Indicates the minimum radius for sharp corners Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinRad(minRad)
Parameters: minRad (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
OvercutColor¶
-
ScrapDesignBuilder.
OvercutColor
¶ Returns or sets the overcut color
-------------------------------------
Getter Method
Signature
OvercutColor()
Returns: Indicates the color of overcuts Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OvercutColor(overcutColor)
Parameters: overcutColor (Id) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
OvercutEdge¶
-
ScrapDesignBuilder.
OvercutEdge
¶ Returns the edge that overcut will be attached
-------------------------------------
Getter Method
Signature
OvercutEdge()
Returns: Return type: NXOpen.SelectEdge
New in version NX6.0.0.
License requirements: None.
OvercutOperation¶
-
ScrapDesignBuilder.
OvercutOperation
¶ Returns or sets the overcut operation, which includes normal type, tangent type, circular type and rectangular type
-------------------------------------
Getter Method
Signature
OvercutOperation()
Returns: Indicates the type of overcut Return type: NXOpen.Tooling.ScrapDesignBuilderOvercutType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OvercutOperation(overcutOperation)
Parameters: overcutOperation ( NXOpen.Tooling.ScrapDesignBuilderOvercutType
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
OverlapColor¶
-
ScrapDesignBuilder.
OverlapColor
¶ Returns or sets the overlap color
-------------------------------------
Getter Method
Signature
OverlapColor()
Returns: Indicates the color of overlaps Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverlapColor(overlapColor)
Parameters: overlapColor (Id) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
OverlapWidth¶
-
ScrapDesignBuilder.
OverlapWidth
¶ Returns or sets the overlap width
-------------------------------------
Getter Method
Signature
OverlapWidth()
Returns: Indicates the width of overlap Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverlapWidth(overlapWidth)
Parameters: overlapWidth (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PierceType¶
-
ScrapDesignBuilder.
PierceType
¶ Returns or sets the piercing type, piercing or piloting
-------------------------------------
Getter Method
Signature
PierceType()
Returns: Indicates the scrap type Return type: NXOpen.Tooling.ScrapDesignBuilderDefScrapType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PierceType(pierceType)
Parameters: pierceType ( NXOpen.Tooling.ScrapDesignBuilderDefScrapType
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PiercingColor¶
-
ScrapDesignBuilder.
PiercingColor
¶ Returns or sets the piercing color
-------------------------------------
Getter Method
Signature
PiercingColor()
Returns: Indicates the color of piercing scraps Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PiercingColor(piercingColor)
Parameters: piercingColor (Id) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PilotingColor¶
-
ScrapDesignBuilder.
PilotingColor
¶ Returns or sets the piloting color
-------------------------------------
Getter Method
Signature
PilotingColor()
Returns: Indicates the color of piloting scraps Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PilotingColor(pilotingColor)
Parameters: pilotingColor (Id) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ProcessFive¶
-
ScrapDesignBuilder.
ProcessFive
¶ Returns or sets the process five
-------------------------------------
Getter Method
Signature
ProcessFive()
Returns: Indicates five steps of trimming process Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProcessFive(processFive)
Parameters: processFive (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ProcessFour¶
-
ScrapDesignBuilder.
ProcessFour
¶ Returns or sets the process four
-------------------------------------
Getter Method
Signature
ProcessFour()
Returns: Indicates four steps of trimming process Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProcessFour(processFour)
Parameters: processFour (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ProcessOne¶
-
ScrapDesignBuilder.
ProcessOne
¶ Returns or sets the process one
-------------------------------------
Getter Method
Signature
ProcessOne()
Returns: Indicates one step of trimming process Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProcessOne(processOne)
Parameters: processOne (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ProcessThree¶
-
ScrapDesignBuilder.
ProcessThree
¶ Returns or sets the process three
-------------------------------------
Getter Method
Signature
ProcessThree()
Returns: Indicates three steps of trimming process Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProcessThree(processThree)
Parameters: processThree (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ProcessTwo¶
-
ScrapDesignBuilder.
ProcessTwo
¶ Returns or sets the process two
-------------------------------------
Getter Method
Signature
ProcessTwo()
Returns: Indicates two steps of trimming process Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProcessTwo(processTwo)
Parameters: processTwo (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemoveFilter¶
-
ScrapDesignBuilder.
RemoveFilter
¶ Returns or sets the removing filter
-------------------------------------
Getter Method
Signature
RemoveFilter()
Returns: Indicates the filter of removing scraps Return type: NXOpen.Tooling.ScrapDesignBuilderRemoveType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RemoveFilter(removeFilter)
Parameters: removeFilter ( NXOpen.Tooling.ScrapDesignBuilderRemoveType
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ScrapMethod¶
-
ScrapDesignBuilder.
ScrapMethod
¶ Returns or sets the scrap method, which includes boundary+sketch, hole boundary, close curves, boundary lines and existed sheet body
-------------------------------------
Getter Method
Signature
ScrapMethod()
Returns: Indicates the creating method of scraps Return type: NXOpen.Tooling.ScrapDesignBuilderScrapDefType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScrapMethod(scrapMethod)
Parameters: scrapMethod ( NXOpen.Tooling.ScrapDesignBuilderScrapDefType
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ScrapPosition¶
-
ScrapDesignBuilder.
ScrapPosition
¶ Returns or sets the scrap position
-------------------------------------
Getter Method
Signature
ScrapPosition()
Returns: Indicates the position method to create scraps Return type: NXOpen.Tooling.ScrapDesignBuilderScrapDefPosition
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScrapPosition(scrapPosition)
Parameters: scrapPosition ( NXOpen.Tooling.ScrapDesignBuilderScrapDefPosition
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ScrapTol¶
-
ScrapDesignBuilder.
ScrapTol
¶ Returns or sets the scrap tolerance, when fail to create scrap in some cases, this value can be decreased to try again
-------------------------------------
Getter Method
Signature
ScrapTol()
Returns: Indicates the tolerance to create scraps Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScrapTol(scrapTol)
Parameters: scrapTol (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ScrapTypeEnum¶
-
ScrapDesignBuilder.
ScrapTypeEnum
¶ Returns or sets the scrap type enum
-------------------------------------
Getter Method
Signature
ScrapTypeEnum()
Returns: Indicates the operating method of scraps Return type: NXOpen.Tooling.ScrapDesignBuilderBody
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScrapTypeEnum(scrapTypeEnum)
Parameters: scrapTypeEnum ( NXOpen.Tooling.ScrapDesignBuilderBody
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondScrap¶
-
ScrapDesignBuilder.
SecondScrap
¶ Returns the second scrap to merge with the first one
-------------------------------------
Getter Method
Signature
SecondScrap()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
SplitCurve¶
-
ScrapDesignBuilder.
SplitCurve
¶ Returns the splitting curve
-------------------------------------
Getter Method
Signature
SplitCurve()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
SplitScrap¶
-
ScrapDesignBuilder.
SplitScrap
¶ Returns the scrap to be splitted or merged
-------------------------------------
Getter Method
Signature
SplitScrap()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
TrimNum¶
-
ScrapDesignBuilder.
TrimNum
¶ Returns or sets the trimming number
-------------------------------------
Getter Method
Signature
TrimNum()
Returns: Indicates the steps of trimming process Return type: NXOpen.Tooling.ScrapDesignBuilderTrimNumType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimNum(trimNum)
Parameters: trimNum ( NXOpen.Tooling.ScrapDesignBuilderTrimNumType
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TrimmingColor¶
-
ScrapDesignBuilder.
TrimmingColor
¶ Returns or sets the trimming color
-------------------------------------
Getter Method
Signature
TrimmingColor()
Returns: Indicates the color of trimming scraps Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimmingColor(trimmingColor)
Parameters: trimmingColor (Id) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
UserAddonCurve¶
-
ScrapDesignBuilder.
UserAddonCurve
¶ Returns the user defined add-on curve to create overlap+overcut
-------------------------------------
Getter Method
Signature
UserAddonCurve()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
Method Detail¶
GetOvercutPosition¶
-
ScrapDesignBuilder.
GetOvercutPosition
¶ Returns the overcut position, it determines where the overcut sketch will be constrained
Signature
GetOvercutPosition()
Returns: Indicates the position to constrain overcut sketch Return type: NXOpen.Point3d
New in version NX6.0.2.
License requirements: None.
SetOvercutPosition¶
-
ScrapDesignBuilder.
SetOvercutPosition
¶ Sets the overcut position, it determines where the overcut sketch will be constrained
Signature
SetOvercutPosition(overcutPosition)
Parameters: overcutPosition ( NXOpen.Point3d
) –New in version NX6.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
ScrapDesignBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.