ScrapDesignBuilderTrimNumType Enumeration¶
NXOpen.Tooling.ScrapDesignBuilder.TrimNumType is an alias for NXOpen.Tooling.ScrapDesignBuilderTrimNumType
-
class
NXOpen.Tooling.
ScrapDesignBuilderTrimNumType
¶ Bases:
object
Specifies the step of trimming process, the maximum is five
Enum Members
Enum Member Enum Member Description One Specifies one step of trimmingTwo Specifies two steps of trimmingThree Specifies three steps of trimmingFour Specifies four steps of trimmingFive Specifies five steps of trimming-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-