ScrapDesignBuilderScrapDefType Enumeration

NXOpen.Tooling.ScrapDesignBuilder.ScrapDefType is an alias for NXOpen.Tooling.ScrapDesignBuilderScrapDefType

class NXOpen.Tooling.ScrapDesignBuilderScrapDefType

Bases: object

Specifies the creation type of scraps

Enum Members

Enum Member Enum Member Description
BlankBoundarySketch
Boundary curves or sketch will be used to create scraps
HoleBoundary
Hole boundary curves will be extracted automatically to create scraps
ClosedCurves
Close curves will be used to create scraps
BoundaryLines
Boundary lines will be used to create an entire scrap
ExistedSheetBody
Existed sheet body will be converted to scrap
ChangeType
The type of scrap will be changed between Piercing and Piloting
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.