ScrapDesignBuilderScrapDefPosition Enumeration

NXOpen.Tooling.ScrapDesignBuilder.ScrapDefPosition is an alias for NXOpen.Tooling.ScrapDesignBuilderScrapDefPosition

class NXOpen.Tooling.ScrapDesignBuilderScrapDefPosition

Bases: object

Specifies the position method of scraps, projecting method is normally used

Enum Members

Enum Member Enum Member Description
ProjectToStrip
Scrap will be projected into the strip plane
KeepOrigin
Scrap will be created in the original plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.