ScrapDesignBuilderOvercutType Enumeration

NXOpen.Tooling.ScrapDesignBuilder.OvercutType is an alias for NXOpen.Tooling.ScrapDesignBuilderOvercutType

class NXOpen.Tooling.ScrapDesignBuilderOvercutType

Bases: object

Specifies the over cut type, different type has different parameters

Enum Members

Enum Member Enum Member Description
NormalType
Creates normal type of overcut
TangentType
Creates tangent type of overcut
CircularType
Creates circular type of overcut
RectangularType
Creates rectangular type of overcut
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.