TrimCurveBuilder Class¶
-
class
NXOpen.Features.
TrimCurveBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.TrimCurve
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateTrimCurveBuilder()
Default values.
Property Value CurveEndOption Start CurveExtensionType Natural CurveOptions.Associative True CurveTrimRegionOption Inside FirstBoundingObjectEndOption Start FirstBoundingObjectOption SelectObject InteresectionDirectionOption RelativeToWcs InteresectionMethod Inferred SecondBoundingObjectEndOption Start SecondBoundingObjectOption SelectObject New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CurveEndOption | Returns or sets the end of the curve that would be trimmed |
CurveExtensionType | Returns or sets the shape of the extension, if the curve to be trimmed is to be extended to its bounding object(s) |
CurveList | Returns the list of curves with the pick points |
CurveOptions | Returns the Curve Options |
CurveTrimRegionOption | Returns or sets the portion of the curves to be trimmed |
CurvesToTrim | Returns the curves to trim |
FirstBoundingObject | Returns the objects for the first boundary against which the selected curves are to be trimmed. |
FirstBoundingObjectEndOption | Returns or sets the end of the first bounding object which would be trimmed |
FirstBoundingObjectOption | Returns or sets the first bounding object option |
FirstBoundingObjectPickPoint | Returns or sets the pick point for the first bounding object |
FirstBoundingPlane | Returns or sets the first bounding object plane |
FirstReferenceIntersection | Returns the first user defined intersection point. |
InteresectionDirectionOption | Returns or sets the method the system uses to find object intersections |
InteresectionMethod | Returns or sets the method to be used to determine the intersections |
InteresectionOptionVector | Returns or sets the vector direction for the trim operation |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReverseTrimEnd | Returns the curves the end to trim needs to be reversed |
SecondBoundingObject | Returns the objects for the second boundary against which the selected curves are to be trimmed. |
SecondBoundingObjectEndOption | Returns or sets the end of the second bounding object which would be trimmed |
SecondBoundingObjectOption | Returns or sets the second bounding object option |
SecondBoundingObjectPickPoint | Returns or sets the pick point for the second bounding object |
SecondBoundingPlane | Returns or sets the first bounding object plane |
SecondReferenceIntersection | Returns the second user defined intersection point. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TrimBoundingObjects | Returns or sets the option whether bounding objects are to be trimmed |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TrimCurveBuilderCurveEndOptions Enumeration | Represents the trim curve end options |
TrimCurveBuilderCurveExtensionTypes Enumeration | Represents the trim curve extension types |
TrimCurveBuilderCurveTrimRegionOptions Enumeration | Represents the trim curve trim region options |
TrimCurveBuilderFirstBoundingObjectEndOptions Enumeration | Represents the trim curve first bounding object end options |
TrimCurveBuilderFirstBoundingObjectOptions Enumeration | Represents the trim curve first bounding object options |
TrimCurveBuilderInteresectionDirectionOptions Enumeration | Represents the trim curve interesection direction options |
TrimCurveBuilderInteresectionMethods Enumeration | Represents the trim curve interesection methods |
TrimCurveBuilderSecondBoundingObjectEndOptions Enumeration | Represents the trim curve second bounding object end options |
TrimCurveBuilderSecondBoundingObjectOptions Enumeration | Represents the trim curve second bounding object options |
Property Detail¶
CurveEndOption¶
-
TrimCurveBuilder.
CurveEndOption
¶ Returns or sets the end of the curve that would be trimmed
-------------------------------------
Getter Method
Signature
CurveEndOption()
Returns: Return type: NXOpen.Features.TrimCurveBuilderCurveEndOptions
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveEndOption(curveEndOption)
Parameters: curveEndOption ( NXOpen.Features.TrimCurveBuilderCurveEndOptions
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
CurveExtensionType¶
-
TrimCurveBuilder.
CurveExtensionType
¶ Returns or sets the shape of the extension, if the curve to be trimmed is to be extended to its bounding object(s)
-------------------------------------
Getter Method
Signature
CurveExtensionType()
Returns: Return type: NXOpen.Features.TrimCurveBuilderCurveExtensionTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveExtensionType(curveExtensionType)
Parameters: curveExtensionType ( NXOpen.Features.TrimCurveBuilderCurveExtensionTypes
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
CurveList¶
-
TrimCurveBuilder.
CurveList
¶ Returns the list of curves with the pick points
-------------------------------------
Getter Method
Signature
CurveList()
Returns: Return type: NXOpen.SelectObjectList
New in version NX5.0.0.
License requirements: None.
CurveOptions¶
-
TrimCurveBuilder.
CurveOptions
¶ Returns the Curve Options
-------------------------------------
Getter Method
Signature
CurveOptions()
Returns: Curve Options Return type: NXOpen.GeometricUtilities.CurveOptions
New in version NX5.0.0.
License requirements: None.
CurveTrimRegionOption¶
-
TrimCurveBuilder.
CurveTrimRegionOption
¶ Returns or sets the portion of the curves to be trimmed
-------------------------------------
Getter Method
Signature
CurveTrimRegionOption()
Returns: Return type: NXOpen.Features.TrimCurveBuilderCurveTrimRegionOptions
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveTrimRegionOption(curveTrimRegionOption)
Parameters: curveTrimRegionOption ( NXOpen.Features.TrimCurveBuilderCurveTrimRegionOptions
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
CurvesToTrim¶
-
TrimCurveBuilder.
CurvesToTrim
¶ Returns the curves to trim
-------------------------------------
Getter Method
Signature
CurvesToTrim()
Returns: Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: None.
FirstBoundingObject¶
-
TrimCurveBuilder.
FirstBoundingObject
¶ Returns the objects for the first boundary against which the selected curves are to be trimmed.
-------------------------------------
Getter Method
Signature
FirstBoundingObject()
Returns: Return type: NXOpen.SelectObjectList
New in version NX5.0.0.
License requirements: None.
FirstBoundingObjectEndOption¶
-
TrimCurveBuilder.
FirstBoundingObjectEndOption
¶ Returns or sets the end of the first bounding object which would be trimmed
-------------------------------------
Getter Method
Signature
FirstBoundingObjectEndOption()
Returns: Return type: NXOpen.Features.TrimCurveBuilderFirstBoundingObjectEndOptions
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstBoundingObjectEndOption(firstBoundingObjectEndOption)
Parameters: firstBoundingObjectEndOption ( NXOpen.Features.TrimCurveBuilderFirstBoundingObjectEndOptions
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
FirstBoundingObjectOption¶
-
TrimCurveBuilder.
FirstBoundingObjectOption
¶ Returns or sets the first bounding object option
-------------------------------------
Getter Method
Signature
FirstBoundingObjectOption()
Returns: Return type: NXOpen.Features.TrimCurveBuilderFirstBoundingObjectOptions
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstBoundingObjectOption(firstBoundingObjectOption)
Parameters: firstBoundingObjectOption ( NXOpen.Features.TrimCurveBuilderFirstBoundingObjectOptions
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
FirstBoundingObjectPickPoint¶
-
TrimCurveBuilder.
FirstBoundingObjectPickPoint
¶ Returns or sets the pick point for the first bounding object
-------------------------------------
Getter Method
Signature
FirstBoundingObjectPickPoint()
Returns: Return type: NXOpen.Point3d
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstBoundingObjectPickPoint(firstBndgObjPickPoint)
Parameters: firstBndgObjPickPoint ( NXOpen.Point3d
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
FirstBoundingPlane¶
-
TrimCurveBuilder.
FirstBoundingPlane
¶ Returns or sets the first bounding object plane
-------------------------------------
Getter Method
Signature
FirstBoundingPlane()
Returns: Return type: NXOpen.Plane
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstBoundingPlane(firstPlane)
Parameters: firstPlane ( NXOpen.Plane
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
FirstReferenceIntersection¶
-
TrimCurveBuilder.
FirstReferenceIntersection
¶ Returns the first user defined intersection point.
-------------------------------------
Getter Method
Signature
FirstReferenceIntersection()
Returns: Return type: NXOpen.SelectPoint
New in version NX5.0.0.
License requirements: None.
InteresectionDirectionOption¶
-
TrimCurveBuilder.
InteresectionDirectionOption
¶ Returns or sets the method the system uses to find object intersections
-------------------------------------
Getter Method
Signature
InteresectionDirectionOption()
Returns: Return type: NXOpen.Features.TrimCurveBuilderInteresectionDirectionOptions
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InteresectionDirectionOption(interesectionDirectionOption)
Parameters: interesectionDirectionOption ( NXOpen.Features.TrimCurveBuilderInteresectionDirectionOptions
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
InteresectionMethod¶
-
TrimCurveBuilder.
InteresectionMethod
¶ Returns or sets the method to be used to determine the intersections
-------------------------------------
Getter Method
Signature
InteresectionMethod()
Returns: Return type: NXOpen.Features.TrimCurveBuilderInteresectionMethods
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InteresectionMethod(interesectionMethod)
Parameters: interesectionMethod ( NXOpen.Features.TrimCurveBuilderInteresectionMethods
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
InteresectionOptionVector¶
-
TrimCurveBuilder.
InteresectionOptionVector
¶ Returns or sets the vector direction for the trim operation
-------------------------------------
Getter Method
Signature
InteresectionOptionVector()
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InteresectionOptionVector(interesectionOptionVector)
Parameters: interesectionOptionVector ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
ReverseTrimEnd¶
-
TrimCurveBuilder.
ReverseTrimEnd
¶ Returns the curves the end to trim needs to be reversed
-------------------------------------
Getter Method
Signature
ReverseTrimEnd()
Returns: Return type: NXOpen.SelectObjectList
New in version NX5.0.0.
License requirements: None.
SecondBoundingObject¶
-
TrimCurveBuilder.
SecondBoundingObject
¶ Returns the objects for the second boundary against which the selected curves are to be trimmed.
-------------------------------------
Getter Method
Signature
SecondBoundingObject()
Returns: Return type: NXOpen.SelectObjectList
New in version NX5.0.0.
License requirements: None.
SecondBoundingObjectEndOption¶
-
TrimCurveBuilder.
SecondBoundingObjectEndOption
¶ Returns or sets the end of the second bounding object which would be trimmed
-------------------------------------
Getter Method
Signature
SecondBoundingObjectEndOption()
Returns: Return type: NXOpen.Features.TrimCurveBuilderSecondBoundingObjectEndOptions
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondBoundingObjectEndOption(secondBoundingObjectEndOption)
Parameters: secondBoundingObjectEndOption ( NXOpen.Features.TrimCurveBuilderSecondBoundingObjectEndOptions
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
SecondBoundingObjectOption¶
-
TrimCurveBuilder.
SecondBoundingObjectOption
¶ Returns or sets the second bounding object option
-------------------------------------
Getter Method
Signature
SecondBoundingObjectOption()
Returns: Return type: NXOpen.Features.TrimCurveBuilderSecondBoundingObjectOptions
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondBoundingObjectOption(secondboundingObjectOption)
Parameters: secondboundingObjectOption ( NXOpen.Features.TrimCurveBuilderSecondBoundingObjectOptions
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
SecondBoundingObjectPickPoint¶
-
TrimCurveBuilder.
SecondBoundingObjectPickPoint
¶ Returns or sets the pick point for the second bounding object
-------------------------------------
Getter Method
Signature
SecondBoundingObjectPickPoint()
Returns: Return type: NXOpen.Point3d
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondBoundingObjectPickPoint(secondBndgObjPickPoint)
Parameters: secondBndgObjPickPoint ( NXOpen.Point3d
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
SecondBoundingPlane¶
-
TrimCurveBuilder.
SecondBoundingPlane
¶ Returns or sets the first bounding object plane
-------------------------------------
Getter Method
Signature
SecondBoundingPlane()
Returns: Return type: NXOpen.Plane
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondBoundingPlane(secondPlane)
Parameters: secondPlane ( NXOpen.Plane
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
SecondReferenceIntersection¶
-
TrimCurveBuilder.
SecondReferenceIntersection
¶ Returns the second user defined intersection point.
-------------------------------------
Getter Method
Signature
SecondReferenceIntersection()
Returns: Return type: NXOpen.SelectPoint
New in version NX5.0.0.
License requirements: None.
TrimBoundingObjects¶
-
TrimCurveBuilder.
TrimBoundingObjects
¶ Returns or sets the option whether bounding objects are to be trimmed
-------------------------------------
Getter Method
Signature
TrimBoundingObjects()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimBoundingObjects(trimBoundingObjects)
Parameters: trimBoundingObjects (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
TrimCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.