TrimCurveBuilderInteresectionMethods Enumeration

NXOpen.Features.TrimCurveBuilder.InteresectionMethods is an alias for NXOpen.Features.TrimCurveBuilderInteresectionMethods

class NXOpen.Features.TrimCurveBuilderInteresectionMethods

Bases: object

Represents the trim curve interesection methods

Enum Members

Enum Member Enum Member Description
Inferred
Inferred
UserDefined
User defined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.