TrimCurveBuilderFirstBoundingObjectEndOptions Enumeration

NXOpen.Features.TrimCurveBuilder.FirstBoundingObjectEndOptions is an alias for NXOpen.Features.TrimCurveBuilderFirstBoundingObjectEndOptions

class NXOpen.Features.TrimCurveBuilderFirstBoundingObjectEndOptions

Bases: object

Represents the trim curve first bounding object end options

Enum Members

Enum Member Enum Member Description
Start
Trim first bounding object from start
End
Trim first bounding object from end
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.