TrimCurveBuilderCurveExtensionTypes Enumeration¶
NXOpen.Features.TrimCurveBuilder.CurveExtensionTypes is an alias for NXOpen.Features.TrimCurveBuilderCurveExtensionTypes
-
class
NXOpen.Features.
TrimCurveBuilderCurveExtensionTypes
¶ Bases:
object
Represents the trim curve extension types
Enum Members
Enum Member Enum Member Description Natural NaturalLinear LinearCircular CircularNotSet None-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-