TrimCurveBuilderInteresectionDirectionOptions Enumeration¶
NXOpen.Features.TrimCurveBuilder.InteresectionDirectionOptions is an alias for NXOpen.Features.TrimCurveBuilderInteresectionDirectionOptions
-
class
NXOpen.Features.
TrimCurveBuilderInteresectionDirectionOptions
¶ Bases:
object
Represents the trim curve interesection direction options
Enum Members
Enum Member Enum Member Description Shortest3dDistance Shortest 3d distanceRelativeToWcs Relative to WCSAlongAVector Along a vectorAlongScreenNormal Along screen normal-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-