EdgeReinforcementBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
EdgeReinforcementBuilder
¶ Bases:
NXOpen.Features.ShipDesign.ProfileSystemBuilder
Represents a
NXOpen.Features.ShipDesign.EdgeReinforcement
builder which is used to create or edit a edge reinforcement system feature.To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateEdgeReinforcementBuilder()
Default values.
Property Value EndCutEnd Connected EndCutStart Connected OrientationAngle.Value 0 OrientationDefinitionBuilder.MeasureAngles NormaltoCurve OrientationDefinitionBuilder.ShowSurfaceAngles 0 OrientationDefinitionBuilder.ShowTwistRate 0 OrientationDefinitionBuilder.ShowWebAngles 0 OrientationMethod FaceNormal StockData.AnchorPoint 0 StockData.PlateHeight.Value 50 (millimeters part), 2 (inches part) StockData.PlateStockData.KnuckleRatio 3.0 StockData.PlateStockData.KnuckleSmoothAngle 3.0 StockData.PlateStockData.MaterialOption 0 StockData.PlateStockData.OppositeThickness.Value 0 (millimeters part), 0 (inches part) StockData.PlateStockData.RestrictThicknessToMaterial true StockData.PlateStockData.ThickenOption SingleSided StockData.PlateStockData.Thickness.Value 10 (millimeters part), 0.5 (inches part) StockData.PlateStockData.ThicknessSourceOption List StockData.SectionType Profile New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the tolerance, in degrees, used to determine when angles are zero. |
Boundary1 | Returns the collector containing the plate system, profile system, or datum plane that will be used to trim the first end of the generated profile system. |
Boundary1Plane | Returns or sets the defined plane that will be used to trim the first end of the generated profile system. |
Boundary2 | Returns the collector containing the plate system, profile system, or datum plane that will be used to trim the second end of the generated profile system. |
Boundary2Plane | Returns or sets the defined plane that will be used to trim the second end of the generated profile system. |
BoundaryReverse | Returns or sets the indication if the side of a single boundary should be changed to the other side or not. |
BuildSolid | Returns or sets the indication of whether to build a solid for the edge reinforcement or just the curve. |
DistanceTolerance | Returns or sets the tolerance used to determine when distances are considered zero. |
Edges | Returns the edges to reinforce. |
EndCutEnd | Returns or sets the end cut to use at the end of the edge reinforcement system. |
EndCutStart | Returns or sets the end cut to use at the start of the edge reinforcement system. |
FirstIntersectionPoints | Returns the selected intersection points between the curves and the first boundary. |
Offset | Returns the offset used for the offset distance from anchor point. |
OrientationAngle | Returns the angle to use for the edge reinforcement orientation. |
OrientationAngleRule | Returns or sets the angle rule to use when measuring angles. |
OrientationDefinitionBuilder | Returns the builder used to define the orientation for the edge reinforcement system. |
OrientationMethod | Returns or sets the method used to orient the edge reinforcement. |
OrientationVector | Returns or sets the orientation vector when the orientation method is NXOpen.Features.ShipDesign.EdgeReinforcementBuilderOrientationMethods.Vector . |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Reverse | Returns or sets the indication if the default direction of the flange is reverse or not. |
ReverseAttachmentDirection | Returns or sets the flag that indicates if the attachment direction is reversed. |
ReversePathDirection | Returns or sets the flag that indicates if the default curve direction should be reversed or not. |
SecondIntersectionPoints | Returns the selected intersection points between the curves and the second boundary. |
ShipNames | Returns the Ship Names builder, used to assign names to the Edge Reinforcement Systems created. |
StockData | Returns the stock data used to define the stock information of the edge reinforcement. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type of placement being used in the edge reinforcement definition. |
Weld | Returns the builder used to specify the welding characteristics for the edge reinforcement. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CreatePathCurves | Creates path curves for all the paths of the profile system. |
CreatePlaneForList | Create a NXOpen.Features.ShipDesign.PlaneListBuilder to add a defined plane to a list. |
DeleteLastPathCurves | Deletes the path curves returned from a call to GetLastPathCurves() . |
DeletePathCurves | Deletes the path curves created from a call to CreatePathCurves() . |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetLastPathCurves | Gets the path curves used by NXOpen.Features.ShipDesign.OrientationDefinitionBuilder . |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetBoundaryOnePoints | Sets the selected intersection points for the first boundary. |
SetBoundaryTwoPoints | Set the selected intersection points for the second boundary. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
EdgeReinforcementBuilderEndCutTypes Enumeration | Used to specify the type of end cut to be used at the extreme ends of the edge reinforcement system. |
EdgeReinforcementBuilderOrientationMethods Enumeration | Used to specify the type of reference to use for specifying the orientation of the edge reinforcement system. |
EdgeReinforcementBuilderTypes Enumeration | Used to specify how the edge reinforcement system is defined. |
Property Detail¶
BuildSolid¶
-
EdgeReinforcementBuilder.
BuildSolid
¶ Returns or sets the indication of whether to build a solid for the edge reinforcement or just the curve.
-------------------------------------
Getter Method
Signature
BuildSolid()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BuildSolid(buildSolid)
Parameters: buildSolid (bool) – New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Edges¶
-
EdgeReinforcementBuilder.
Edges
¶ Returns the edges to reinforce.
-------------------------------------
Getter Method
Signature
Edges()
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: None.
EndCutEnd¶
-
EdgeReinforcementBuilder.
EndCutEnd
¶ Returns or sets the end cut to use at the end of the edge reinforcement system.
-------------------------------------
Getter Method
Signature
EndCutEnd()
Returns: Return type: NXOpen.Features.ShipDesign.EdgeReinforcementBuilderEndCutTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCutEnd(endCutEnd)
Parameters: endCutEnd ( NXOpen.Features.ShipDesign.EdgeReinforcementBuilderEndCutTypes
) –New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
EndCutStart¶
-
EdgeReinforcementBuilder.
EndCutStart
¶ Returns or sets the end cut to use at the start of the edge reinforcement system.
-------------------------------------
Getter Method
Signature
EndCutStart()
Returns: Return type: NXOpen.Features.ShipDesign.EdgeReinforcementBuilderEndCutTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCutStart(endCutStart)
Parameters: endCutStart ( NXOpen.Features.ShipDesign.EdgeReinforcementBuilderEndCutTypes
) –New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Offset¶
-
EdgeReinforcementBuilder.
Offset
¶ Returns the offset used for the offset distance from anchor point.
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OrientationAngle¶
-
EdgeReinforcementBuilder.
OrientationAngle
¶ Returns the angle to use for the edge reinforcement orientation.
-------------------------------------
Getter Method
Signature
OrientationAngle()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OrientationDefinitionBuilder¶
-
EdgeReinforcementBuilder.
OrientationDefinitionBuilder
¶ Returns the builder used to define the orientation for the edge reinforcement system.
-------------------------------------
Getter Method
Signature
OrientationDefinitionBuilder()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationDefinitionBuilder
New in version NX9.0.0.
License requirements: None.
OrientationMethod¶
-
EdgeReinforcementBuilder.
OrientationMethod
¶ Returns or sets the method used to orient the edge reinforcement.
-------------------------------------
Getter Method
Signature
OrientationMethod()
Returns: Return type: NXOpen.Features.ShipDesign.EdgeReinforcementBuilderOrientationMethods
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationMethod(orientationMethod)
Parameters: orientationMethod ( NXOpen.Features.ShipDesign.EdgeReinforcementBuilderOrientationMethods
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
OrientationVector¶
-
EdgeReinforcementBuilder.
OrientationVector
¶ Returns or sets the orientation vector when the orientation method is
NXOpen.Features.ShipDesign.EdgeReinforcementBuilderOrientationMethods.Vector
.-------------------------------------
Getter Method
Signature
OrientationVector()
Returns: Return type: NXOpen.Direction
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationVector(orientationVector)
Parameters: orientationVector ( NXOpen.Direction
) –New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Reverse¶
-
EdgeReinforcementBuilder.
Reverse
¶ Returns or sets the indication if the default direction of the flange is reverse or not.
-------------------------------------
Getter Method
Signature
Reverse()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Reverse(reverse)
Parameters: reverse (bool) – New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
ReverseAttachmentDirection¶
-
EdgeReinforcementBuilder.
ReverseAttachmentDirection
¶ Returns or sets the flag that indicates if the attachment direction is reversed.
-------------------------------------
Getter Method
Signature
ReverseAttachmentDirection()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseAttachmentDirection(reverse)
Parameters: reverse (bool) – New in version NX10.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
ShipNames¶
-
EdgeReinforcementBuilder.
ShipNames
¶ Returns the Ship Names builder, used to assign names to the Edge Reinforcement Systems created.
-------------------------------------
Getter Method
Signature
ShipNames()
Returns: Ship Names Builder Return type: NXOpen.Features.ShipDesign.ShipNamesBuilder
New in version NX9.0.2.
License requirements: None.
StockData¶
-
EdgeReinforcementBuilder.
StockData
¶ Returns the stock data used to define the stock information of the edge reinforcement.
-------------------------------------
Getter Method
Signature
StockData()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerStockBuilder
New in version NX8.0.0.
License requirements: None.
Type¶
-
EdgeReinforcementBuilder.
Type
¶ Returns or sets the type of placement being used in the edge reinforcement definition.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.ShipDesign.EdgeReinforcementBuilderTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.ShipDesign.EdgeReinforcementBuilderTypes
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Weld¶
-
EdgeReinforcementBuilder.
Weld
¶ Returns the builder used to specify the welding characteristics for the edge reinforcement.
-------------------------------------
Getter Method
Signature
Weld()
Returns: Return type: NXOpen.Weld.CharacteristicsBuilder
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
EdgeReinforcementBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.