StiffenerStockBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
StiffenerStockBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class defines the Profile or Plate stock for a Stiffener or Edge Reinforcement feature.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AnchorPoint | Returns or sets the anchor point for profiles only. |
BuiltUpStockData | Returns the built-up stock data |
PlateHeight | Returns the plate height |
PlateStockData | Returns the plate stock data |
ProfileStockData | Returns the profile stock data |
SectionType | Returns or sets the section type (profile or plate) |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetAvailableAnchorPointNames | The list of available anchor points @return Array of available anchor point names. |
PopulateAnchorPointList | Update anchor points |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StiffenerStockBuilderStockSectionType Enumeration | Type of Stiffener/Edge Reinforcement stock: Profile or Plate |
Property Detail¶
AnchorPoint¶
-
StiffenerStockBuilder.
AnchorPoint
¶ Returns or sets the anchor point for profiles only.
-------------------------------------
Getter Method
Signature
AnchorPoint()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnchorPoint(anchorPoint)
Parameters: anchorPoint (int) – New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
BuiltUpStockData¶
-
StiffenerStockBuilder.
BuiltUpStockData
¶ Returns the built-up stock data
-------------------------------------
Getter Method
Signature
BuiltUpStockData()
Returns: Return type: NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
New in version NX9.0.0.
License requirements: None.
PlateHeight¶
-
StiffenerStockBuilder.
PlateHeight
¶ Returns the plate height
-------------------------------------
Getter Method
Signature
PlateHeight()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
PlateStockData¶
-
StiffenerStockBuilder.
PlateStockData
¶ Returns the plate stock data
-------------------------------------
Getter Method
Signature
PlateStockData()
Returns: Return type: NXOpen.Features.ShipDesign.PlateStockBuilder
New in version NX8.0.0.
License requirements: None.
ProfileStockData¶
-
StiffenerStockBuilder.
ProfileStockData
¶ Returns the profile stock data
-------------------------------------
Getter Method
Signature
ProfileStockData()
Returns: Return type: NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
New in version NX8.0.0.
License requirements: None.
SectionType¶
-
StiffenerStockBuilder.
SectionType
¶ Returns or sets the section type (profile or plate)
-------------------------------------
Getter Method
Signature
SectionType()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerStockBuilderStockSectionType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionType(sectionType)
Parameters: sectionType ( NXOpen.Features.ShipDesign.StiffenerStockBuilderStockSectionType
) –New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
Method Detail¶
GetAvailableAnchorPointNames¶
-
StiffenerStockBuilder.
GetAvailableAnchorPointNames
¶ The list of available anchor points
Signature
GetAvailableAnchorPointNames()
Returns: Array of available anchor point names. These names are read from the current reuse sketch :rtype: list of str
New in version NX8.0.0.
License requirements: None.
PopulateAnchorPointList¶
-
StiffenerStockBuilder.
PopulateAnchorPointList
¶ Update anchor points
Signature
PopulateAnchorPointList()
New in version NX9.0.0.
License requirements: None.
Validate¶
-
StiffenerStockBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.