OrientationDefinitionBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
OrientationDefinitionBuilder
¶ Bases:
NXOpen.Builder
This class defines the top level object for use in definining the orientation of stiffeners and edge reinforcements.
This object allows you to define regions of a profile and allows you to define a different method of orientation for each region. To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateOrientationDefinitionBuilder()
Default values.
Property Value MeasureAngles NormaltoCurve ShowSurfaceAngles 0 ShowTwistRate 0 ShowWebAngles 0 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance used in the orientation objects to determine if vectors are parallel. |
DistanceTolerance | Returns or sets the distance tolerance used in the orientation objects to determine if locations are coincident. |
MeasureAngles | Returns or sets the method in which to measure angles in the orientation objects. |
NewRegionPoint | Returns the new region point or datum that will be used for the boundary of the new region. |
PlacementSide | Returns or sets the side of the placement faces the stiffener is to be placed upon. |
RegionItemData | Returns the regionItem builder. |
RegionList | Returns the list containing all the defined regions. |
ShowSurfaceAngles | Returns or sets the indication if the surface angles analysis display is on or off. |
ShowTwistRate | Returns or sets the indication if the twist rate analysis display is on or off. |
ShowWebAngles | Returns or sets the indication if the web angle analysis display is on or off. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateNewRegion | Creates a new region on the landing curve to allow you to change the orientation for this area of the landing curve. |
CreatePathCurve | Sets the landing curve that is being processed into the builder. |
CreateRegionsAtFrames | Will create new regions at each frame. |
DeleteRegion | Deletes a previously created region. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetNextRegion | Gets the next region to the current one. |
GetObject | Returns the object currently being edited by this builder. |
SetAnglesNormal | Will set all angle values of input regions so that web is normal to surface. |
SetPlacementFaces | Sets the faces or datum that are being processed into the builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
OrientationDefinitionBuilderMeasureAngleTypes Enumeration | Settings to indicate how angles are measured in all orientation objects. |
OrientationDefinitionBuilderPlacementSideTypes Enumeration | Settings to indicate which side of the placement faces the stiffener is to be placed. |
Property Detail¶
AngleTolerance¶
-
OrientationDefinitionBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance used in the orientation objects to determine if vectors are parallel.
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance(tolerance)
Parameters: tolerance (float) – New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
DistanceTolerance¶
-
OrientationDefinitionBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance used in the orientation objects to determine if locations are coincident.
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(tolerance)
Parameters: tolerance (float) – New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
MeasureAngles¶
-
OrientationDefinitionBuilder.
MeasureAngles
¶ Returns or sets the method in which to measure angles in the orientation objects.
-------------------------------------
Getter Method
Signature
MeasureAngles()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationDefinitionBuilderMeasureAngleTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeasureAngles(measureAngles)
Parameters: measureAngles ( NXOpen.Features.ShipDesign.OrientationDefinitionBuilderMeasureAngleTypes
) –New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
NewRegionPoint¶
-
OrientationDefinitionBuilder.
NewRegionPoint
¶ Returns the new region point or datum that will be used for the boundary of the new region.
-------------------------------------
Getter Method
Signature
NewRegionPoint()
Returns: Return type: NXOpen.SelectNXObject
New in version NX9.0.0.
License requirements: None.
PlacementSide¶
-
OrientationDefinitionBuilder.
PlacementSide
¶ Returns or sets the side of the placement faces the stiffener is to be placed upon.
-------------------------------------
Getter Method
Signature
PlacementSide()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationDefinitionBuilderPlacementSideTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlacementSide(placementSide)
Parameters: placementSide ( NXOpen.Features.ShipDesign.OrientationDefinitionBuilderPlacementSideTypes
) –New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
RegionItemData¶
-
OrientationDefinitionBuilder.
RegionItemData
¶ Returns the regionItem builder.
-------------------------------------
Getter Method
Signature
RegionItemData()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationRegionItemBuilder
New in version NX9.0.0.
License requirements: None.
RegionList¶
-
OrientationDefinitionBuilder.
RegionList
¶ Returns the list containing all the defined regions.
-------------------------------------
Getter Method
Signature
RegionList()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationRegionItemBuilderList
New in version NX9.0.0.
License requirements: None.
ShowSurfaceAngles¶
-
OrientationDefinitionBuilder.
ShowSurfaceAngles
¶ Returns or sets the indication if the surface angles analysis display is on or off.
-------------------------------------
Getter Method
Signature
ShowSurfaceAngles()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowSurfaceAngles(showSurfaceAngles)
Parameters: showSurfaceAngles (bool) – New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
ShowTwistRate¶
-
OrientationDefinitionBuilder.
ShowTwistRate
¶ Returns or sets the indication if the twist rate analysis display is on or off.
-------------------------------------
Getter Method
Signature
ShowTwistRate()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowTwistRate(showTwistRate)
Parameters: showTwistRate (bool) – New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
ShowWebAngles¶
-
OrientationDefinitionBuilder.
ShowWebAngles
¶ Returns or sets the indication if the web angle analysis display is on or off.
-------------------------------------
Getter Method
Signature
ShowWebAngles()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowWebAngles(showWebAngles)
Parameters: showWebAngles (bool) – New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
Method Detail¶
CreateNewRegion¶
-
OrientationDefinitionBuilder.
CreateNewRegion
¶ Creates a new region on the landing curve to allow you to change the orientation for this area of the landing curve.
Signature
CreateNewRegion(regionPoint)
Parameters: regionPoint ( NXOpen.NXObject
) – New region boundary pointReturns: Return type: NXOpen.Features.ShipDesign.OrientationRegionItemBuilder
New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
CreatePathCurve¶
-
OrientationDefinitionBuilder.
CreatePathCurve
¶ Sets the landing curve that is being processed into the builder.
If regions have already been defined the closest point on this new curve to the region boundaries will be used for the new region boundaries when the boundary has been defined by a specified point otherwise the boundary definition will be reevaluated for this new curve and the boundary set appropriately.
Signature
CreatePathCurve(curves)
Parameters: curves (list of NXOpen.NXObject
) – The curves defining the path of the profile that is being oriented.New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
CreateRegionsAtFrames¶
-
OrientationDefinitionBuilder.
CreateRegionsAtFrames
¶ Will create new regions at each frame.
Signature
CreateRegionsAtFrames()
Returns: The regions created. Return type: list of NXOpen.Features.ShipDesign.OrientationRegionItemBuilder
New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
DeleteRegion¶
-
OrientationDefinitionBuilder.
DeleteRegion
¶ Deletes a previously created region.
The deleted region will be combined with the previous region.
Signature
DeleteRegion(region)
Parameters: region ( NXOpen.Features.ShipDesign.OrientationRegionItemBuilder
) –New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
GetNextRegion¶
-
OrientationDefinitionBuilder.
GetNextRegion
¶ Gets the next region to the current one.
Signature
GetNextRegion(region)
Parameters: region ( NXOpen.Features.ShipDesign.OrientationRegionItemBuilder
) –Returns: Return type: NXOpen.Features.ShipDesign.OrientationRegionItemBuilder
New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
SetAnglesNormal¶
-
OrientationDefinitionBuilder.
SetAnglesNormal
¶ Will set all angle values of input regions so that web is normal to surface.
Signature
SetAnglesNormal(regions)
Parameters: regions (list of NXOpen.Features.ShipDesign.OrientationRegionItemBuilder
) – The regions to process.New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
SetPlacementFaces¶
-
OrientationDefinitionBuilder.
SetPlacementFaces
¶ Sets the faces or datum that are being processed into the builder.
Signature
SetPlacementFaces(faces)
Parameters: faces (list of NXOpen.DisplayableObject
) – The faces/datums defining the placement of the profile that is being oriented.New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
Validate¶
-
OrientationDefinitionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.