OrientationDefinitionBuilderPlacementSideTypes Enumeration¶
NXOpen.Features.ShipDesign.OrientationDefinitionBuilder.PlacementSideTypes is an alias for NXOpen.Features.ShipDesign.OrientationDefinitionBuilderPlacementSideTypes
-
class
NXOpen.Features.ShipDesign.
OrientationDefinitionBuilderPlacementSideTypes
¶ Bases:
object
Settings to indicate which side of the placement faces the stiffener is to be placed.
Enum Members
- placement faces. “
- “OppositeNormal”, ” The stiffener will be placed on the negative normal side of the
placement faces. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.