OrientationRegionItemBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
OrientationRegionItemBuilder
¶ Bases:
NXOpen.Builder
This class defines each region of the orientation.
To create a new instance of this class, use
NXOpen.Features.ShipDesign.OrientationDefinitionBuilder.CreateNewRegion()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AngleMethods | Returns the angle definition for the region’s orientation. |
EndAngleMethods | Returns the angle definition for the end of this region’s orientation. |
EndPointMethods | Returns the boundary definition at the end of this region. |
OrientationMethod | Returns or sets the orientation method used to define the direction of the web for this region. |
StartAngleMethods | Returns the angle definition for the start of this region’s orientation. |
StartPointMethods | Returns the boundary definition at the start of this region. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
OrientationRegionItemBuilderOrientationMethodTypes Enumeration | Settings to indicate how the web orientation is defined for this region. |
Property Detail¶
AngleMethods¶
-
OrientationRegionItemBuilder.
AngleMethods
¶ Returns the angle definition for the region’s orientation.
Only used when OrientationMethod is
Features.ShipDesign.OrientationRegionItemBuilderOrientationMethodTypes.NormalToSurface
,Features.ShipDesign.OrientationRegionItemBuilderOrientationMethodTypes.Orthogonal
,Features.ShipDesign.OrientationRegionItemBuilderOrientationMethodTypes.AlongVector
, orFeatures.ShipDesign.OrientationRegionItemBuilderOrientationMethodTypes.PlanarAtAngle
-------------------------------------
Getter Method
Signature
AngleMethods()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilder
New in version NX9.0.0.
License requirements: None.
EndAngleMethods¶
-
OrientationRegionItemBuilder.
EndAngleMethods
¶ Returns the angle definition for the end of this region’s orientation.
Only used when OrientationMethod is
Features.ShipDesign.OrientationRegionItemBuilderOrientationMethodTypes.LinearTwist
, ofFeatures.ShipDesign.OrientationRegionItemBuilderOrientationMethodTypes.CubicTwist
.-------------------------------------
Getter Method
Signature
EndAngleMethods()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilder
New in version NX9.0.0.
License requirements: None.
EndPointMethods¶
-
OrientationRegionItemBuilder.
EndPointMethods
¶ Returns the boundary definition at the end of this region.
Note this is NULL for the last region. The object output is the same as the start of the following region.
-------------------------------------
Getter Method
Signature
EndPointMethods()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationPointMethodsBuilder
New in version NX9.0.0.
License requirements: None.
OrientationMethod¶
-
OrientationRegionItemBuilder.
OrientationMethod
¶ Returns or sets the orientation method used to define the direction of the web for this region.
-------------------------------------
Getter Method
Signature
OrientationMethod()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationRegionItemBuilderOrientationMethodTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationMethod(orientationMethod)
Parameters: orientationMethod ( NXOpen.Features.ShipDesign.OrientationRegionItemBuilderOrientationMethodTypes
) –New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
StartAngleMethods¶
-
OrientationRegionItemBuilder.
StartAngleMethods
¶ Returns the angle definition for the start of this region’s orientation.
Only used when OrientationMethod is
Features.ShipDesign.OrientationRegionItemBuilderOrientationMethodTypes.LinearTwist
, ofFeatures.ShipDesign.OrientationRegionItemBuilderOrientationMethodTypes.CubicTwist
.-------------------------------------
Getter Method
Signature
StartAngleMethods()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilder
New in version NX9.0.0.
License requirements: None.
StartPointMethods¶
-
OrientationRegionItemBuilder.
StartPointMethods
¶ Returns the boundary definition at the start of this region.
Note this is NULL for the first region. The object output is the same as the end of the previous region.
-------------------------------------
Getter Method
Signature
StartPointMethods()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationPointMethodsBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
OrientationRegionItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.