OrientationAngleMethodsBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
OrientationAngleMethodsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class defines the method of angle definition used in the definition of the region’s orientation.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AlignAt | Returns or sets the indication if the region should be aligned with the adjacent region at the start of this region, or with the adjacent region at the end of this region. |
AlignVector | Returns or sets the vector used to calculate the angle by aligning to this vector. |
AngleMethod | Returns or sets the method used to calculate the angle. |
AngleReference | Returns or sets the object used to measure the angle from. |
MountingAngle | Returns the constant angle value to rotate from the given vector or reference object. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
OrientationAngleMethodsBuilderAlignAtTypes Enumeration | Is the angle to be aligned with the region adjacent to start of this region or adjacent to the end of this region. |
OrientationAngleMethodsBuilderMethodTypes Enumeration | Settings used to determine how the angle is defined. |
Property Detail¶
AlignAt¶
-
OrientationAngleMethodsBuilder.
AlignAt
¶ Returns or sets the indication if the region should be aligned with the adjacent region at the start of this region, or with the adjacent region at the end of this region.
Only used when
NXOpen.Features.ShipDesign.OrientationRegionItemBuilder.OrientationMethodTypes()
isFeatures.ShipDesign.OrientationRegionItemBuilderOrientationMethodTypes.PlanarAtAngle
.-------------------------------------
Getter Method
Signature
AlignAt()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilderAlignAtTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignAt(alignAt)
Parameters: alignAt ( NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilderAlignAtTypes
) –New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
AlignVector¶
-
OrientationAngleMethodsBuilder.
AlignVector
¶ Returns or sets the vector used to calculate the angle by aligning to this vector.
Only used when AngleMethod is
Features.ShipDesign.OrientationAngleMethodsBuilderMethodTypes.Vector
.-------------------------------------
Getter Method
Signature
AlignVector()
Returns: Return type: NXOpen.Direction
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignVector(alignVector)
Parameters: alignVector ( NXOpen.Direction
) –New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
AngleMethod¶
-
OrientationAngleMethodsBuilder.
AngleMethod
¶ Returns or sets the method used to calculate the angle.
-------------------------------------
Getter Method
Signature
AngleMethod()
Returns: Return type: NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilderMethodTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleMethod(angleMethod)
Parameters: angleMethod ( NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilderMethodTypes
) –New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
AngleReference¶
-
OrientationAngleMethodsBuilder.
AngleReference
¶ Returns or sets the object used to measure the angle from.
Only used when AngleMethod is
Features.ShipDesign.OrientationAngleMethodsBuilderMethodTypes.Angle
.-------------------------------------
Getter Method
Signature
AngleReference()
Returns: Return type: NXOpen.Plane
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleReference(angleReference)
Parameters: angleReference ( NXOpen.Plane
) –New in version NX9.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
MountingAngle¶
-
OrientationAngleMethodsBuilder.
MountingAngle
¶ Returns the constant angle value to rotate from the given vector or reference object.
-------------------------------------
Getter Method
Signature
MountingAngle()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
OrientationAngleMethodsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.