OrientationAngleMethodsBuilderMethodTypes Enumeration¶
NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilder.MethodTypes is an alias for NXOpen.Features.ShipDesign.OrientationAngleMethodsBuilderMethodTypes
-
class
NXOpen.Features.ShipDesign.
OrientationAngleMethodsBuilderMethodTypes
¶ Bases:
object
Settings used to determine how the angle is defined.
Enum Members
Enum Member Enum Member Description Angle Angle is defined by specifying a constant angle from a reference object.Vector Angle is defined by specifying a vector to align with.Aligned Angle is the same as the previous or following region.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-