OrientationDefinitionBuilderMeasureAngleTypes Enumeration¶
NXOpen.Features.ShipDesign.OrientationDefinitionBuilder.MeasureAngleTypes is an alias for NXOpen.Features.ShipDesign.OrientationDefinitionBuilderMeasureAngleTypes
-
class
NXOpen.Features.ShipDesign.
OrientationDefinitionBuilderMeasureAngleTypes
¶ Bases:
object
Settings to indicate how angles are measured in all orientation objects.
Enum Members
landing curve. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-