ShipNamesBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ShipNamesBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class provides the mechanism for defining the names of Basic Design objects such as Decks, Bulkheads, Stiffener Systems, etc.
Each Ship object type (Deck, etc.) has a specific format for the names defined in a “recipes” files located at UGII_BASE_DIR/nxship/data/ShipNamesRecipes.xml.
A recipe is composed of two or more “fields”. Individual fields are defined via a :py:class:`NXOpen.Features.ShipDesign.ShipNameFieldBuilder`object.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ContextAttribute | Returns or sets the Context Attribute value. |
ShipObjectType | Returns or sets the Ship object type (Hull, Deck, etc. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetField | Get the ShipNameField at the given index (starting at 0) @return |
GetFieldcount | Get the number of ShipNameFields in this recipe @return |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ContextAttribute¶
-
ShipNamesBuilder.
ContextAttribute
¶ Returns or sets the Context Attribute value.
This is the value of the SAW_SUB_NAME part attribute added to the newly created / named Ship objects.
-------------------------------------
Getter Method
Signature
ContextAttribute()
Returns: Return type: str New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContextAttribute(newValue)
Parameters: newValue (str) – New in version NX9.0.2.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
ShipObjectType¶
-
ShipNamesBuilder.
ShipObjectType
¶ Returns or sets the Ship object type (Hull, Deck, etc.
) for which names will be generated.
-------------------------------------
Getter Method
Signature
ShipObjectType()
Returns: Return type: NXOpen.Features.ShipDesign.ShipnamesBuilderType
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShipObjectType(type)
Parameters: type ( NXOpen.Features.ShipDesign.ShipnamesBuilderType
) –New in version NX9.0.2.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
Method Detail¶
GetField¶
-
ShipNamesBuilder.
GetField
¶ Get the ShipNameField at the given index (starting at 0)
Signature
GetField(idx)
Parameters: idx (int) – Returns: Return type: NXOpen.Features.ShipDesign.ShipNameFieldBuilder
New in version NX9.0.2.
License requirements: None.
GetFieldcount¶
-
ShipNamesBuilder.
GetFieldcount
¶ Get the number of ShipNameFields in this recipe
Signature
GetFieldcount()
Returns: Return type: int New in version NX9.0.2.
License requirements: None.
Validate¶
-
ShipNamesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.