ShipNameFieldBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ShipNameFieldBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
A field, combined with other fields, to generate a name for a Ship Basic Design Object such as a Deck.
The ShipNameFieldBuilder class contains the information used to generate a name for a Basic Design object, such as a Deck, Bulkhead, Stiffener System, etc. <code> Fields can be one of four types: 1) Fixed A string with an unchangeable value 2) Any A user entered string value 3) Option A predefined set of strings from which the user can choose one 4) Index A system generated, leading zeros, number which pretends to provide name uniqueness. </code> There may be as many Fixed, Any, and Option fields as the user deems appropriate. There may be only one Index field.
The fields for a particular Ship object type
NXOpen.Features.ShipDesign.ShipNamesBuilder
are defined in a “recipes” file which specifies, for a particular object type, the fields and their values. See ShipNamesRecipes.xml in UGII_BASE_DIR/nxship/data for details on the recipes. <code> A sample recipe might be defined having the following fields:Type Value ——– ——– Fixed “TBH-” Option “Port”, “Starboard”, “None” Fixed “-” Index nnnnnn</code>
This is an abstract class and cannot be instantiated
New in version NX9.0.2.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Value | Returns or sets the field value. |
Methods¶
Method | Description |
---|---|
GetOptionValues | Get the valid option values for an Option type field. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Value¶
-
ShipNameFieldBuilder.
Value
¶ Returns or sets the field value.
-------------------------------------
Getter Method
Signature
Value()
Returns: Return type: str New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Value(newValue)
Parameters: newValue (str) – New in version NX9.0.2.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
Method Detail¶
GetOptionValues¶
-
ShipNameFieldBuilder.
GetOptionValues
¶ Get the valid option values for an Option type field.
No values are returned (and the count is set to zero) if this is not an option field
Signature
GetOptionValues()
Returns: Return type: list of str New in version NX9.0.2.
License requirements: None.
Validate¶
-
ShipNameFieldBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.