SectionSurfaceBuilder Class¶
-
class
NXOpen.Features.
SectionSurfaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.SectionSurface
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateSectionSurfaceBuilder()
Default values.
Property Value AngleLaw.EndValue.Value 1 AngleLaw.Function ft AngleLaw.LawType Constant AngleLaw.Parameter t AngleLaw.StartValue.Value 1 AngleLaw.Value.Value 0.0 EndContinuity.ContinuityType G1 RadiusLaw.EndValue.Value 1.0 (millimeters part), 0.05 (inches part) RadiusLaw.StartValue.Value 1.0 (millimeters part), 0.05 (inches part) RadiusLaw.Value.Value 1.0 (millimeters part), 0.05 (inches part) RhoLaw.EndValue.Value 0.5 RhoLaw.StartValue.Value 0.5 RhoLaw.Value.Value 0.5 SectionMethodCircularTangent FilletArc SectionMethodFilletBridge Continuity SectionMethodRho Rho StartContinuity.ContinuityType G1 New in version NX5.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Features.SectionSurfaceBuilderEx
instead.
Properties¶
Property | Description |
---|---|
AlternateMethod | Returns or sets the alternate method. |
AngleLaw | Returns the angle Law |
ApexCurve | Returns the apex curve. |
ControlRegion | Returns or sets the control region for fillet bridge |
CreateApexCurve | Returns or sets whether an apex curve should be created |
CurvatureTolerance | Returns or sets the curvature tolerance |
EndContinuity | Returns the end continuity for fillet bridge |
EndDepthSkew | Returns the end depth and skew |
EndFlowDirection | Returns or sets the end flow direction for fillet bridge |
EndGuide | Returns the end guide |
EndHighlightSection | Returns the end highlight section . |
EndShapeCurve | Returns the end shape curve for fillet bridge |
EndSlope | Returns the end slope. |
EndSurface | Returns the end surface Only applies to the follow section surface types: NXOpen.Features.SectionSurfaceBuilderTypes.FilletShoulder , NXOpen.Features.SectionSurfaceBuilderTypes.FilletRho , NXOpen.Features.SectionSurfaceBuilderTypes.FilletHilite and NXOpen.Features.SectionSurfaceBuilderTypes.FilletBridge |
EntireRegionDepthSkew | Returns the entire region depth and skew |
InteriorGuide1 | Returns the interior guide1. |
InteriorGuide2 | Returns the interior guide2 Only applies to the follow section surface types: NXOpen.Features.SectionSurfaceBuilderTypes.FourPointSlope and NXOpen.Features.SectionSurfaceBuilderTypes.FivePoint |
InteriorGuide3 | Returns the interior guide3 Only applies to the follow section surface types: NXOpen.Features.SectionSurfaceBuilderTypes.FourPointSlope and NXOpen.Features.SectionSurfaceBuilderTypes.FivePoint |
OrientationGuide | Returns the orientation guide. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PositionTolerance | Returns or sets the position tolerance |
RadiusLaw | Returns the radius Law |
ReverseEndSurface | Returns or sets the reverse end surface Only applies to the follow section surface types: NXOpen.Features.SectionSurfaceBuilderTypes.PointRadiusAngleArc and NXOpen.Features.SectionSurfaceBuilderTypes.FilletBridge |
ReverseStartDirection | Returns or sets the reverse start direction. |
RhoLaw | Returns the rho Law |
SectionMethodCircularTangent | Returns or sets the section method for circular tangent |
SectionMethodFilletBridge | Returns or sets the section method for fillet bridge |
SectionMethodRho | Returns or sets the section method for rho law |
Shoulder | Returns the shoulder. |
SpineCurve | Returns the spine curve |
StartContinuity | Returns the start continuity for fillet bridge |
StartDepthSkew | Returns the start depth and skew |
StartFlowDirection | Returns or sets the start flow direction for fillet bridge |
StartGuide | Returns the start guide |
StartHighlightSection | Returns the start highlight section. |
StartShapeCurve | Returns the start shape curve for fillet bridge |
StartSlope | Returns the start slope. |
StartSurface | Returns the start surface. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TangentTolerance | Returns or sets the tangent tolerance |
Type | Returns or sets the type |
UDegree | Returns or sets the u degree |
VDegree | Returns the v degree |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SectionSurfaceBuilderControlRegionEnum Enumeration | This enum represents the type of the region where depth and skew can be applied |
SectionSurfaceBuilderFlowDirectionEnum Enumeration | This enum represents the type of flow direction for the start/end of the section surface |
SectionSurfaceBuilderSectionMethodCircularTangentEnum Enumeration | This enum represents the current types of section method for circular tangent method |
SectionSurfaceBuilderSectionMethodFilletBridgeEnum Enumeration | This enum represents the current types of section method for fillet bridge method |
SectionSurfaceBuilderSectionMethodRhoEnum Enumeration | This enum represents the current types of section method for section methods with rho law |
SectionSurfaceBuilderTypes Enumeration | This enum represents the current types of section surface methods |
SectionSurfaceBuilderUDegreeEnum Enumeration | This enum represents the current types of section surface in u direction |
Property Detail¶
AlternateMethod¶
-
SectionSurfaceBuilder.
AlternateMethod
¶ Returns or sets the alternate method.
This api only applies to the follow section surface methods, circle_tangent and linear-tangent
-------------------------------------
Getter Method
Signature
AlternateMethod()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlternateMethod(alternateMethod)
Parameters: alternateMethod (int) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
AngleLaw¶
-
SectionSurfaceBuilder.
AngleLaw
¶ Returns the angle Law
-------------------------------------
Getter Method
Signature
AngleLaw()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX6.0.0.
License requirements: None.
ApexCurve¶
-
SectionSurfaceBuilder.
ApexCurve
¶ Returns the apex curve.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.EndsApexShoulder
,NXOpen.Features.SectionSurfaceBuilderTypes.EndsApexRho
, andNXOpen.Features.SectionSurfaceBuilderTypes.EndsApexHilite
-------------------------------------
Getter Method
Signature
ApexCurve()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
ControlRegion¶
-
SectionSurfaceBuilder.
ControlRegion
¶ Returns or sets the control region for fillet bridge
-------------------------------------
Getter Method
Signature
ControlRegion()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderControlRegionEnum
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ControlRegion(controlRegion)
Parameters: controlRegion ( NXOpen.Features.SectionSurfaceBuilderControlRegionEnum
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
CreateApexCurve¶
-
SectionSurfaceBuilder.
CreateApexCurve
¶ Returns or sets whether an apex curve should be created
-------------------------------------
Getter Method
Signature
CreateApexCurve()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateApexCurve(createApexCurve)
Parameters: createApexCurve (bool) – New in version NX5.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”), solid_modeling (“SOLIDS MODELING”)
CurvatureTolerance¶
-
SectionSurfaceBuilder.
CurvatureTolerance
¶ Returns or sets the curvature tolerance
-------------------------------------
Getter Method
Signature
CurvatureTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
-------------------------------------
Setter Method
Signature
CurvatureTolerance(curvatureTolerance)
Parameters: curvatureTolerance (float) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
EndContinuity¶
-
SectionSurfaceBuilder.
EndContinuity
¶ Returns the end continuity for fillet bridge
-------------------------------------
Getter Method
Signature
EndContinuity()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
EndDepthSkew¶
-
SectionSurfaceBuilder.
EndDepthSkew
¶ Returns the end depth and skew
-------------------------------------
Getter Method
Signature
EndDepthSkew()
Returns: Return type: NXOpen.GeometricUtilities.DepthSkewBuilder
New in version NX6.0.0.
License requirements: None.
EndFlowDirection¶
-
SectionSurfaceBuilder.
EndFlowDirection
¶ Returns or sets the end flow direction for fillet bridge
-------------------------------------
Getter Method
Signature
EndFlowDirection()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderFlowDirectionEnum
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndFlowDirection(endFlowDirection)
Parameters: endFlowDirection ( NXOpen.Features.SectionSurfaceBuilderFlowDirectionEnum
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
EndGuide¶
-
SectionSurfaceBuilder.
EndGuide
¶ Returns the end guide
-------------------------------------
Getter Method
Signature
EndGuide()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
EndHighlightSection¶
-
SectionSurfaceBuilder.
EndHighlightSection
¶ Returns the end highlight section .
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.EndsApexHilite
,NXOpen.Features.SectionSurfaceBuilderTypes.EndsSlopeHilite
andNXOpen.Features.SectionSurfaceBuilderTypes.FilletHilite
-------------------------------------
Getter Method
Signature
EndHighlightSection()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
EndShapeCurve¶
-
SectionSurfaceBuilder.
EndShapeCurve
¶ Returns the end shape curve for fillet bridge
-------------------------------------
Getter Method
Signature
EndShapeCurve()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
EndSlope¶
-
SectionSurfaceBuilder.
EndSlope
¶ Returns the end slope.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.EndsSlopeShoulder
,NXOpen.Features.SectionSurfaceBuilderTypes.EndsSlopeRho
,NXOpen.Features.SectionSurfaceBuilderTypes.EndsSlopeHilite
,NXOpen.Features.SectionSurfaceBuilderTypes.EndsSlopeCubic
andNXOpen.Features.SectionSurfaceBuilderTypes.FourPointSlope
-------------------------------------
Getter Method
Signature
EndSlope()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
EndSurface¶
-
SectionSurfaceBuilder.
EndSurface
¶ Returns the end surface Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.FilletShoulder
,NXOpen.Features.SectionSurfaceBuilderTypes.FilletRho
,NXOpen.Features.SectionSurfaceBuilderTypes.FilletHilite
andNXOpen.Features.SectionSurfaceBuilderTypes.FilletBridge
-------------------------------------
Getter Method
Signature
EndSurface()
Returns: Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: None.
EntireRegionDepthSkew¶
-
SectionSurfaceBuilder.
EntireRegionDepthSkew
¶ Returns the entire region depth and skew
-------------------------------------
Getter Method
Signature
EntireRegionDepthSkew()
Returns: Return type: NXOpen.GeometricUtilities.DepthSkewBuilder
New in version NX6.0.0.
License requirements: None.
InteriorGuide1¶
-
SectionSurfaceBuilder.
InteriorGuide1
¶ Returns the interior guide1.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.FourPointSlope
,NXOpen.Features.SectionSurfaceBuilderTypes.FivePoint
, andNXOpen.Features.SectionSurfaceBuilderTypes.ThreePointArc
-------------------------------------
Getter Method
Signature
InteriorGuide1()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
InteriorGuide2¶
-
SectionSurfaceBuilder.
InteriorGuide2
¶ Returns the interior guide2 Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.FourPointSlope
andNXOpen.Features.SectionSurfaceBuilderTypes.FivePoint
-------------------------------------
Getter Method
Signature
InteriorGuide2()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
InteriorGuide3¶
-
SectionSurfaceBuilder.
InteriorGuide3
¶ Returns the interior guide3 Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.FourPointSlope
andNXOpen.Features.SectionSurfaceBuilderTypes.FivePoint
-------------------------------------
Getter Method
Signature
InteriorGuide3()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
OrientationGuide¶
-
SectionSurfaceBuilder.
OrientationGuide
¶ Returns the orientation guide.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.Circle
-------------------------------------
Getter Method
Signature
OrientationGuide()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
PositionTolerance¶
-
SectionSurfaceBuilder.
PositionTolerance
¶ Returns or sets the position tolerance
-------------------------------------
Getter Method
Signature
PositionTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
-------------------------------------
Setter Method
Signature
PositionTolerance(positionTolerance)
Parameters: positionTolerance (float) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
RadiusLaw¶
-
SectionSurfaceBuilder.
RadiusLaw
¶ Returns the radius Law
-------------------------------------
Getter Method
Signature
RadiusLaw()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX6.0.0.
License requirements: None.
ReverseEndSurface¶
-
SectionSurfaceBuilder.
ReverseEndSurface
¶ Returns or sets the reverse end surface Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.PointRadiusAngleArc
andNXOpen.Features.SectionSurfaceBuilderTypes.FilletBridge
-------------------------------------
Getter Method
Signature
ReverseEndSurface()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseEndSurface(reverseEndSurface)
Parameters: reverseEndSurface (bool) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
ReverseStartDirection¶
-
SectionSurfaceBuilder.
ReverseStartDirection
¶ Returns or sets the reverse start direction.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.PointRadiusAngleArc
andNXOpen.Features.SectionSurfaceBuilderTypes.FilletBridge
-------------------------------------
Getter Method
Signature
ReverseStartDirection()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseStartDirection(reverseStartDirection)
Parameters: reverseStartDirection (bool) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
RhoLaw¶
-
SectionSurfaceBuilder.
RhoLaw
¶ Returns the rho Law
-------------------------------------
Getter Method
Signature
RhoLaw()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX6.0.0.
License requirements: None.
SectionMethodCircularTangent¶
-
SectionSurfaceBuilder.
SectionMethodCircularTangent
¶ Returns or sets the section method for circular tangent
-------------------------------------
Getter Method
Signature
SectionMethodCircularTangent()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderSectionMethodCircularTangentEnum
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionMethodCircularTangent(sectionMethodCircularTangent)
Parameters: sectionMethodCircularTangent ( NXOpen.Features.SectionSurfaceBuilderSectionMethodCircularTangentEnum
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
SectionMethodFilletBridge¶
-
SectionSurfaceBuilder.
SectionMethodFilletBridge
¶ Returns or sets the section method for fillet bridge
-------------------------------------
Getter Method
Signature
SectionMethodFilletBridge()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderSectionMethodFilletBridgeEnum
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionMethodFilletBridge(sectionMethodFilletBridge)
Parameters: sectionMethodFilletBridge ( NXOpen.Features.SectionSurfaceBuilderSectionMethodFilletBridgeEnum
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
SectionMethodRho¶
-
SectionSurfaceBuilder.
SectionMethodRho
¶ Returns or sets the section method for rho law
-------------------------------------
Getter Method
Signature
SectionMethodRho()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderSectionMethodRhoEnum
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionMethodRho(sectionMethodRho)
Parameters: sectionMethodRho ( NXOpen.Features.SectionSurfaceBuilderSectionMethodRhoEnum
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
Shoulder¶
-
SectionSurfaceBuilder.
Shoulder
¶ Returns the shoulder.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.EndsApexShoulder
,NXOpen.Features.SectionSurfaceBuilderTypes.EndsSlopeShoulder
andNXOpen.Features.SectionSurfaceBuilderTypes.FilletShoulder
-------------------------------------
Getter Method
Signature
Shoulder()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
SpineCurve¶
-
SectionSurfaceBuilder.
SpineCurve
¶ Returns the spine curve
-------------------------------------
Getter Method
Signature
SpineCurve()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
StartContinuity¶
-
SectionSurfaceBuilder.
StartContinuity
¶ Returns the start continuity for fillet bridge
-------------------------------------
Getter Method
Signature
StartContinuity()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
StartDepthSkew¶
-
SectionSurfaceBuilder.
StartDepthSkew
¶ Returns the start depth and skew
-------------------------------------
Getter Method
Signature
StartDepthSkew()
Returns: Return type: NXOpen.GeometricUtilities.DepthSkewBuilder
New in version NX6.0.0.
License requirements: None.
StartFlowDirection¶
-
SectionSurfaceBuilder.
StartFlowDirection
¶ Returns or sets the start flow direction for fillet bridge
-------------------------------------
Getter Method
Signature
StartFlowDirection()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderFlowDirectionEnum
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartFlowDirection(startFlowDirection)
Parameters: startFlowDirection ( NXOpen.Features.SectionSurfaceBuilderFlowDirectionEnum
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
StartGuide¶
-
SectionSurfaceBuilder.
StartGuide
¶ Returns the start guide
-------------------------------------
Getter Method
Signature
StartGuide()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
StartHighlightSection¶
-
SectionSurfaceBuilder.
StartHighlightSection
¶ Returns the start highlight section.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.EndsApexHilite
,NXOpen.Features.SectionSurfaceBuilderTypes.EndsSlopeHilite
andNXOpen.Features.SectionSurfaceBuilderTypes.FilletHilite
-------------------------------------
Getter Method
Signature
StartHighlightSection()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
StartShapeCurve¶
-
SectionSurfaceBuilder.
StartShapeCurve
¶ Returns the start shape curve for fillet bridge
-------------------------------------
Getter Method
Signature
StartShapeCurve()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
StartSlope¶
-
SectionSurfaceBuilder.
StartSlope
¶ Returns the start slope.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.EndsSlopeShoulder
,NXOpen.Features.SectionSurfaceBuilderTypes.EndsSlopeRho
,NXOpen.Features.SectionSurfaceBuilderTypes.EndsSlopeHilite
,NXOpen.Features.SectionSurfaceBuilderTypes.EndsSlopeCubic
andNXOpen.Features.SectionSurfaceBuilderTypes.FourPointSlope
-------------------------------------
Getter Method
Signature
StartSlope()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
StartSurface¶
-
SectionSurfaceBuilder.
StartSurface
¶ Returns the start surface.
Only applies to the follow section surface types:
NXOpen.Features.SectionSurfaceBuilderTypes.FilletShoulder
,NXOpen.Features.SectionSurfaceBuilderTypes.FilletRho
,NXOpen.Features.SectionSurfaceBuilderTypes.FilletHilite
andNXOpen.Features.SectionSurfaceBuilderTypes.FilletBridge
-------------------------------------
Getter Method
Signature
StartSurface()
Returns: Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: None.
TangentTolerance¶
-
SectionSurfaceBuilder.
TangentTolerance
¶ Returns or sets the tangent tolerance
-------------------------------------
Getter Method
Signature
TangentTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
-------------------------------------
Setter Method
Signature
TangentTolerance(tangentTolerance)
Parameters: tangentTolerance (float) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
Type¶
-
SectionSurfaceBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.SectionSurfaceBuilderTypes
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
UDegree¶
-
SectionSurfaceBuilder.
UDegree
¶ Returns or sets the u degree
-------------------------------------
Getter Method
Signature
UDegree()
Returns: Return type: NXOpen.Features.SectionSurfaceBuilderUDegreeEnum
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UDegree(uDegree)
Parameters: uDegree ( NXOpen.Features.SectionSurfaceBuilderUDegreeEnum
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_2 (“advanced freeform modeling”)
VDegree¶
-
SectionSurfaceBuilder.
VDegree
¶ Returns the v degree
-------------------------------------
Getter Method
Signature
VDegree()
Returns: Return type: NXOpen.GeometricUtilities.Rebuild
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SectionSurfaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.