SectionSurfaceBuilderSectionMethodRhoEnum Enumeration

NXOpen.Features.SectionSurfaceBuilder.SectionMethodRhoEnum is an alias for NXOpen.Features.SectionSurfaceBuilderSectionMethodRhoEnum

class NXOpen.Features.SectionSurfaceBuilderSectionMethodRhoEnum

Bases: object

This enum represents the current types of section method for section methods with rho law

Enum Members

Enum Member Enum Member Description
Rho
rho law method
LeastTension
least tension method
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.