SectionSurfaceBuilderControlRegionEnum Enumeration

NXOpen.Features.SectionSurfaceBuilder.ControlRegionEnum is an alias for NXOpen.Features.SectionSurfaceBuilderControlRegionEnum

class NXOpen.Features.SectionSurfaceBuilderControlRegionEnum

Bases: object

This enum represents the type of the region where depth and skew can be applied

Enum Members

Enum Member Enum Member Description
Entire
depth and skew applied to the entire section surface
Start
depth and skew applied to the start section of the section surface
End
depth and skew applied to the end section of the section surface
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.