SectionSurfaceBuilderSectionMethodCircularTangentEnum Enumeration

NXOpen.Features.SectionSurfaceBuilder.SectionMethodCircularTangentEnum is an alias for NXOpen.Features.SectionSurfaceBuilderSectionMethodCircularTangentEnum

class NXOpen.Features.SectionSurfaceBuilderSectionMethodCircularTangentEnum

Bases: object

This enum represents the current types of section method for circular tangent method

Enum Members

Enum Member Enum Member Description
FilletArc
fillet arc
CoverArc
cover arc
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.