AutomotiveCollection Class

class NXOpen.Features.AutomotiveCollection

Bases: object

This class contains the factory method for creating automotive feature builder.

To obtain an instance of this class, refer to NXOpen.Features.FeatureCollection

New in version NX7.5.0.

Methods

Method Description
CreateAllAroundVisionBuilder Creates a NXOpen.Features.VehicleDesign.AllAroundVisionBuilder @return
CreateBaseDataBuilder Creates a NXOpen.Features.VehicleDesign.BaseDataBuilder @return
CreateBaseDataImportExportBuilder Creates a NXOpen.Features.VehicleDesign.BaseDataImportExportBuilder @return
CreateBumperPendulumBuilder Creates a NXOpen.Features.VehicleDesign.BumperPendulumBuilder @return
CreateCloseRangeVisibilityBuilder Creates a NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilder @return
CreateCrashBarrierBuilder Creates a NXOpen.Features.VehicleDesign.CrashBarrierBuilder @return
CreateDynamicCurbBuilder Creates a NXOpen.Features.VehicleDesign.DynamicCurbBuilder @return
CreateGroundClearanceBuilder Creates a NXOpen.Features.VehicleDesign.GroundClearanceBuilder @return
CreateHeadImpactApillarBuilder Creates a NXOpen.Features.VehicleDesign.HeadImpactAPillarBuilder @return
CreateHeadImpactBpillarBuilder Creates a NXOpen.Features.VehicleDesign.HeadImpactBPillarBuilder @return
CreateHeadImpactBuilder Creates a NXOpen.Features.VehicleDesign.HeadImpactBuilder @return
CreateHeadImpactFrontHeaderBuilder Creates a NXOpen.Features.VehicleDesign.HeadImpactFrontHeaderBuilder @return
CreateHeadImpactOpillarBuilder Creates a NXOpen.Features.VehicleDesign.HeadImpactOPillarBuilder @return
CreateHeadImpactOtherRailBuilder Creates a NXOpen.Features.VehicleDesign.HeadImpactOtherRailBuilder @return
CreateHeadImpactRearHeaderBuilder Creates a NXOpen.Features.VehicleDesign.HeadImpactRearHeaderBuilder @return
CreateHeadImpactRpillarBuilder Creates a NXOpen.Features.VehicleDesign.HeadImpactRPillarBuilder @return
CreateHeadImpactSideRailBuilder Creates a NXOpen.Features.VehicleDesign.HeadImpactSideRailBuilder @return
CreateHeadImpactUpperRoofBuilder Creates a NXOpen.Features.VehicleDesign.HeadImpactUpperRoofBuilder @return
CreateInnerAngleBuilder Creates a NXOpen.Features.VehicleDesign.InnerAngleBuilder @return
CreateManikinBuilder Creates a NXOpen.Features.VehicleDesign.ManikinBuilder @return
CreateMirrorCertificationBuilder Creates a NXOpen.Features.VehicleDesign.MirrorCertificationBuilder @return
CreateOilPanBuilder Creates a NXOpen.Features.VehicleDesign.OilPanBuilder @return
CreatePedestrianProtectionBuilder Creates a NXOpen.Features.VehicleDesign.PedestrianProtectionBuilder @return
CreateSlopeBuilder Creates a NXOpen.Features.VehicleDesign.SlopeBuilder @return
CreateStaticCurbBuilder Creates a NXOpen.Features.VehicleDesign.StaticCurbBuilder @return
CreateTireEnvelopeBuilder Creates a NXOpen.Features.VehicleDesign.TireEnvelopeBuilder @return
CreateVisionPlaneBuilder Creates a NXOpen.Features.VehicleDesign.VisionPlaneBuilder @return
CreateWheelCoveringBuilder Creates a NXOpen.Features.VehicleDesign.WheelCoveringBuilder @return
CreateWheelFixingBuilder Creates a NXOpen.Features.VehicleDesign.WheelFixingBuilder @return
CreateWindshieldDatumBuilder Creates a NXOpen.Features.VehicleDesign.WindshieldDatumBuilder @return

Method Detail

CreateAllAroundVisionBuilder

AutomotiveCollection.CreateAllAroundVisionBuilder

Creates a NXOpen.Features.VehicleDesign.AllAroundVisionBuilder

Signature CreateAllAroundVisionBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateAllAroundVisionBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateBaseDataBuilder

AutomotiveCollection.CreateBaseDataBuilder

Creates a NXOpen.Features.VehicleDesign.BaseDataBuilder

Signature CreateBaseDataBuilder()

Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateBaseDataBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateBaseDataImportExportBuilder

AutomotiveCollection.CreateBaseDataImportExportBuilder

Creates a NXOpen.Features.VehicleDesign.BaseDataImportExportBuilder

Signature CreateBaseDataImportExportBuilder()

Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateBaseDataImportExportBuilder() instead.

License requirements: gateway (“UG GATEWAY”)

CreateBumperPendulumBuilder

AutomotiveCollection.CreateBumperPendulumBuilder

Creates a NXOpen.Features.VehicleDesign.BumperPendulumBuilder

Signature CreateBumperPendulumBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateBumperPendulumBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateCloseRangeVisibilityBuilder

AutomotiveCollection.CreateCloseRangeVisibilityBuilder

Creates a NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilder

Signature CreateCloseRangeVisibilityBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateCloseRangeVisibilityBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateCrashBarrierBuilder

AutomotiveCollection.CreateCrashBarrierBuilder

Creates a NXOpen.Features.VehicleDesign.CrashBarrierBuilder

Signature CreateCrashBarrierBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateCrashBarrierBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateDynamicCurbBuilder

AutomotiveCollection.CreateDynamicCurbBuilder

Creates a NXOpen.Features.VehicleDesign.DynamicCurbBuilder

Signature CreateDynamicCurbBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateDynamicCurbBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateGroundClearanceBuilder

AutomotiveCollection.CreateGroundClearanceBuilder

Creates a NXOpen.Features.VehicleDesign.GroundClearanceBuilder

Signature CreateGroundClearanceBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateGroundClearanceBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateHeadImpactApillarBuilder

AutomotiveCollection.CreateHeadImpactApillarBuilder

Creates a NXOpen.Features.VehicleDesign.HeadImpactAPillarBuilder

Signature CreateHeadImpactApillarBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateHeadImpactApillarBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateHeadImpactBpillarBuilder

AutomotiveCollection.CreateHeadImpactBpillarBuilder

Creates a NXOpen.Features.VehicleDesign.HeadImpactBPillarBuilder

Signature CreateHeadImpactBpillarBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateHeadImpactBpillarBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateHeadImpactBuilder

AutomotiveCollection.CreateHeadImpactBuilder

Creates a NXOpen.Features.VehicleDesign.HeadImpactBuilder

Signature CreateHeadImpactBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateHeadImpactBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateHeadImpactFrontHeaderBuilder

AutomotiveCollection.CreateHeadImpactFrontHeaderBuilder

Creates a NXOpen.Features.VehicleDesign.HeadImpactFrontHeaderBuilder

Signature CreateHeadImpactFrontHeaderBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateHeadImpactFrontHeaderBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateHeadImpactOpillarBuilder

AutomotiveCollection.CreateHeadImpactOpillarBuilder

Creates a NXOpen.Features.VehicleDesign.HeadImpactOPillarBuilder

Signature CreateHeadImpactOpillarBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateHeadImpactOpillarBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateHeadImpactOtherRailBuilder

AutomotiveCollection.CreateHeadImpactOtherRailBuilder

Creates a NXOpen.Features.VehicleDesign.HeadImpactOtherRailBuilder

Signature CreateHeadImpactOtherRailBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateHeadImpactOtherRailBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateHeadImpactRearHeaderBuilder

AutomotiveCollection.CreateHeadImpactRearHeaderBuilder

Creates a NXOpen.Features.VehicleDesign.HeadImpactRearHeaderBuilder

Signature CreateHeadImpactRearHeaderBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateHeadImpactRearHeaderBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateHeadImpactRpillarBuilder

AutomotiveCollection.CreateHeadImpactRpillarBuilder

Creates a NXOpen.Features.VehicleDesign.HeadImpactRPillarBuilder

Signature CreateHeadImpactRpillarBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateHeadImpactRpillarBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateHeadImpactSideRailBuilder

AutomotiveCollection.CreateHeadImpactSideRailBuilder

Creates a NXOpen.Features.VehicleDesign.HeadImpactSideRailBuilder

Signature CreateHeadImpactSideRailBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateHeadImpactSideRailBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateHeadImpactUpperRoofBuilder

AutomotiveCollection.CreateHeadImpactUpperRoofBuilder

Creates a NXOpen.Features.VehicleDesign.HeadImpactUpperRoofBuilder

Signature CreateHeadImpactUpperRoofBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateHeadImpactUpperRoofBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateInnerAngleBuilder

AutomotiveCollection.CreateInnerAngleBuilder

Creates a NXOpen.Features.VehicleDesign.InnerAngleBuilder

Signature CreateInnerAngleBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateInnerAngleBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateManikinBuilder

AutomotiveCollection.CreateManikinBuilder

Creates a NXOpen.Features.VehicleDesign.ManikinBuilder

Signature CreateManikinBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX7.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateManikinBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateMirrorCertificationBuilder

AutomotiveCollection.CreateMirrorCertificationBuilder

Creates a NXOpen.Features.VehicleDesign.MirrorCertificationBuilder

Signature CreateMirrorCertificationBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateMirrorCertificationBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateOilPanBuilder

AutomotiveCollection.CreateOilPanBuilder

Creates a NXOpen.Features.VehicleDesign.OilPanBuilder

Signature CreateOilPanBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateOilPanBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreatePedestrianProtectionBuilder

AutomotiveCollection.CreatePedestrianProtectionBuilder

Creates a NXOpen.Features.VehicleDesign.PedestrianProtectionBuilder

Signature CreatePedestrianProtectionBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreatePedestrianProtectionBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateSlopeBuilder

AutomotiveCollection.CreateSlopeBuilder

Creates a NXOpen.Features.VehicleDesign.SlopeBuilder

Signature CreateSlopeBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateSlopeBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateStaticCurbBuilder

AutomotiveCollection.CreateStaticCurbBuilder

Creates a NXOpen.Features.VehicleDesign.StaticCurbBuilder

Signature CreateStaticCurbBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateStaticCurbBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateTireEnvelopeBuilder

AutomotiveCollection.CreateTireEnvelopeBuilder

Creates a NXOpen.Features.VehicleDesign.TireEnvelopeBuilder

Signature CreateTireEnvelopeBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX7.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateTireEnvelopeBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateVisionPlaneBuilder

AutomotiveCollection.CreateVisionPlaneBuilder

Creates a NXOpen.Features.VehicleDesign.VisionPlaneBuilder

Signature CreateVisionPlaneBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateVisionPlaneBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateWheelCoveringBuilder

AutomotiveCollection.CreateWheelCoveringBuilder

Creates a NXOpen.Features.VehicleDesign.WheelCoveringBuilder

Signature CreateWheelCoveringBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateWheelCoveringBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateWheelFixingBuilder

AutomotiveCollection.CreateWheelFixingBuilder

Creates a NXOpen.Features.VehicleDesign.WheelFixingBuilder

Signature CreateWheelFixingBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX8.5.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateWheelFixingBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)

CreateWindshieldDatumBuilder

AutomotiveCollection.CreateWindshieldDatumBuilder

Creates a NXOpen.Features.VehicleDesign.WindshieldDatumBuilder

Signature CreateWindshieldDatumBuilder(feature)

Parameters:feature (NXOpen.Features.Feature) – feature to be edited
Returns:
Return type:NXOpen.Features.FeatureBuilder

New in version NX9.0.0.

Deprecated since version NX9.0.0: Use Features.VehicleDesignCollection.CreateWindshieldDatumBuilder() instead.

License requirements: nx_general_packaging (“NX General Packaging”)