HeadImpactBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
HeadImpactBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.HeadImpactBuilder
.To create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateHeadImpactBuilder()
Default values.
Property Value ActiveZone 0 COGFrontXOffset.Value 0 (millimeters part), 0 (inches part) COGFrontZOffset.Value 0 (millimeters part), 0 (inches part) COGRearXOffset.Value 0 (millimeters part), 0 (inches part) COGRearZOffset.Value 0 (millimeters part), 0 (inches part) Calculation BothSides RequirementsControl StandardDriven VisualizeZone 0 ZoneDistance.Value 0 (millimeters part), 0 (inches part) New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
APillarFeature | Returns or sets the a-pillar feature for this head impact study. |
ActiveZone | Returns or sets the activate exclusion zone flag for this head impact study. |
BPillarFeature | Returns or sets the b-pillar feature for this head impact study. |
COGFrontXOffset | Returns the center of gravity front longitudunal offset for this head impact study. |
COGFrontZOffset | Returns the center of gravity front vertical offset for this head impact study. |
COGRearXOffset | Returns the center of gravity rear longitudunal offset for this head impact study. |
COGRearZOffset | Returns the center of gravity rear vertical offset for this head impact study. |
Calculation | Returns or sets the calculation type for this head impact study. |
FrontHeaderFeature | Returns or sets the front header feature for this head impact study. |
Loading | Returns or sets the loading used for this head impact study. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RPillarFeature | Returns or sets the rear pillar feature for this head impact study. |
RearHeaderFeature | Returns or sets the rear header feature for this head impact study. |
RequirementsControl | Returns or sets the requirements control for standard driven or user defined. |
SideRailFeature | Returns or sets the side rail feature for this head impact study. |
Standard | Returns or sets the standard used for this head impact study. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
UpperRoofFeature | Returns or sets the upper roof feature for this head impact study. |
VisualizeZone | Returns or sets the visualize exclusion zone flag for this head impact study. |
ZoneDistance | Returns the exclusion zone distance for this head impact study. |
Methods¶
Method | Description |
---|---|
AddAdditionalPillarFeature | The method to add an additional pillar feature. |
AddAdditionalRailFeature | The method to add an additional side rail feature. |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
HeadImpactBuilderCalculationType Enumeration | Represents the calculation types. |
HeadImpactBuilderRequirementsControlType Enumeration | Represents the requirements control types. |
Property Detail¶
APillarFeature¶
-
HeadImpactBuilder.
APillarFeature
¶ Returns or sets the a-pillar feature for this head impact study.
-------------------------------------
Getter Method
Signature
APillarFeature()
Returns: Return type: NXOpen.Features.VehicleDesign.HeadImpactAPillar
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
APillarFeature(feature)
Parameters: feature ( NXOpen.Features.VehicleDesign.HeadImpactAPillar
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ActiveZone¶
-
HeadImpactBuilder.
ActiveZone
¶ Returns or sets the activate exclusion zone flag for this head impact study.
-------------------------------------
Getter Method
Signature
ActiveZone()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveZone(activeZone)
Parameters: activeZone (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
BPillarFeature¶
-
HeadImpactBuilder.
BPillarFeature
¶ Returns or sets the b-pillar feature for this head impact study.
-------------------------------------
Getter Method
Signature
BPillarFeature()
Returns: Return type: NXOpen.Features.VehicleDesign.HeadImpactBPillar
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BPillarFeature(feature)
Parameters: feature ( NXOpen.Features.VehicleDesign.HeadImpactBPillar
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
COGFrontXOffset¶
-
HeadImpactBuilder.
COGFrontXOffset
¶ Returns the center of gravity front longitudunal offset for this head impact study.
-------------------------------------
Getter Method
Signature
COGFrontXOffset()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
COGFrontZOffset¶
-
HeadImpactBuilder.
COGFrontZOffset
¶ Returns the center of gravity front vertical offset for this head impact study.
-------------------------------------
Getter Method
Signature
COGFrontZOffset()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
COGRearXOffset¶
-
HeadImpactBuilder.
COGRearXOffset
¶ Returns the center of gravity rear longitudunal offset for this head impact study.
-------------------------------------
Getter Method
Signature
COGRearXOffset()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
COGRearZOffset¶
-
HeadImpactBuilder.
COGRearZOffset
¶ Returns the center of gravity rear vertical offset for this head impact study.
-------------------------------------
Getter Method
Signature
COGRearZOffset()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
Calculation¶
-
HeadImpactBuilder.
Calculation
¶ Returns or sets the calculation type for this head impact study.
-------------------------------------
Getter Method
Signature
Calculation()
Returns: Return type: NXOpen.Features.VehicleDesign.HeadImpactBuilderCalculationType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Calculation(calculation)
Parameters: calculation ( NXOpen.Features.VehicleDesign.HeadImpactBuilderCalculationType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FrontHeaderFeature¶
-
HeadImpactBuilder.
FrontHeaderFeature
¶ Returns or sets the front header feature for this head impact study.
-------------------------------------
Getter Method
Signature
FrontHeaderFeature()
Returns: Return type: NXOpen.Features.VehicleDesign.HeadImpactFrontHeader
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrontHeaderFeature(feature)
Parameters: feature ( NXOpen.Features.VehicleDesign.HeadImpactFrontHeader
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Loading¶
-
HeadImpactBuilder.
Loading
¶ Returns or sets the loading used for this head impact study.
-------------------------------------
Getter Method
Signature
Loading()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Loading(loading)
Parameters: loading (str) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RPillarFeature¶
-
HeadImpactBuilder.
RPillarFeature
¶ Returns or sets the rear pillar feature for this head impact study.
-------------------------------------
Getter Method
Signature
RPillarFeature()
Returns: Return type: NXOpen.Features.VehicleDesign.HeadImpactRPillar
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RPillarFeature(feature)
Parameters: feature ( NXOpen.Features.VehicleDesign.HeadImpactRPillar
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearHeaderFeature¶
-
HeadImpactBuilder.
RearHeaderFeature
¶ Returns or sets the rear header feature for this head impact study.
-------------------------------------
Getter Method
Signature
RearHeaderFeature()
Returns: Return type: NXOpen.Features.VehicleDesign.HeadImpactRearHeader
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RearHeaderFeature(feature)
Parameters: feature ( NXOpen.Features.VehicleDesign.HeadImpactRearHeader
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RequirementsControl¶
-
HeadImpactBuilder.
RequirementsControl
¶ Returns or sets the requirements control for standard driven or user defined.
-------------------------------------
Getter Method
Signature
RequirementsControl()
Returns: Return type: NXOpen.Features.VehicleDesign.HeadImpactBuilderRequirementsControlType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RequirementsControl(requirementsControl)
Parameters: requirementsControl ( NXOpen.Features.VehicleDesign.HeadImpactBuilderRequirementsControlType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SideRailFeature¶
-
HeadImpactBuilder.
SideRailFeature
¶ Returns or sets the side rail feature for this head impact study.
-------------------------------------
Getter Method
Signature
SideRailFeature()
Returns: Return type: NXOpen.Features.VehicleDesign.HeadImpactSideRail
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SideRailFeature(feature)
Parameters: feature ( NXOpen.Features.VehicleDesign.HeadImpactSideRail
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Standard¶
-
HeadImpactBuilder.
Standard
¶ Returns or sets the standard used for this head impact study.
-------------------------------------
Getter Method
Signature
Standard()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Standard(standard)
Parameters: standard (str) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
UpperRoofFeature¶
-
HeadImpactBuilder.
UpperRoofFeature
¶ Returns or sets the upper roof feature for this head impact study.
-------------------------------------
Getter Method
Signature
UpperRoofFeature()
Returns: Return type: NXOpen.Features.VehicleDesign.HeadImpactUpperRoof
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperRoofFeature(feature)
Parameters: feature ( NXOpen.Features.VehicleDesign.HeadImpactUpperRoof
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
VisualizeZone¶
-
HeadImpactBuilder.
VisualizeZone
¶ Returns or sets the visualize exclusion zone flag for this head impact study.
-------------------------------------
Getter Method
Signature
VisualizeZone()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeZone(visualizeZone)
Parameters: visualizeZone (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ZoneDistance¶
-
HeadImpactBuilder.
ZoneDistance
¶ Returns the exclusion zone distance for this head impact study.
-------------------------------------
Getter Method
Signature
ZoneDistance()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
Method Detail¶
AddAdditionalPillarFeature¶
-
HeadImpactBuilder.
AddAdditionalPillarFeature
¶ The method to add an additional pillar feature.
Signature
AddAdditionalPillarFeature(feature)
Parameters: feature ( NXOpen.Features.VehicleDesign.HeadImpactOPillar
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
AddAdditionalRailFeature¶
-
HeadImpactBuilder.
AddAdditionalRailFeature
¶ The method to add an additional side rail feature.
Signature
AddAdditionalRailFeature(feature)
Parameters: feature ( NXOpen.Features.VehicleDesign.HeadImpactOtherRail
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Validate¶
-
HeadImpactBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.