GroundClearanceBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
GroundClearanceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.GroundClearance
builder.To create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateGroundClearanceBuilder()
Default values.
Property Value DistanceToRoadGeneral.Value 200 (millimeters part), 7.9 (inches part) DistanceToRoadUnderAxle.Value 100 (millimeters part), 3.9 (inches part) ExtendSurface 0 ExtensionFactor.Value 1000 Position Front RequirementsControl StandardDriven SectionCurve HorizontalLine ShowDistanceMeasurement 1 SurfaceLength FrontToRear UseGeneralSurface 1 UseUnderAxleSurface 1 Visualization Surface WheelSize StaticRadius New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
DistanceToRoadGeneral | Returns the expression that contains the value which indicates the distance from general surface to road general. |
DistanceToRoadUnderAxle | Returns the expression that contains the value which indicates the distance from the under axle surface to road. |
ExtendSurface | Returns or sets the indication if use surface extension. |
ExtensionFactor | Returns the expression that contains the value which indicates the extension factor. |
FrontUnderAxleFace | Returns the faces representing the car body geometry for measuring distance to the front under axle surface. |
GeneralClearanceFace | Returns the faces representing the car body geometry for measuring distance to the general surface. |
Loading | Returns or sets the loading to be applied. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Position | Returns or sets the position of the under axle surface. |
RearUnderAxleFace | Returns the faces representing the car body geometry for measuring distance to the rear under axle surface. |
RequirementsControl | Returns or sets the value to determine what type of requirement is controlling the ground clearance values. |
SectionCurve | Returns or sets the section curve type of the under axle surface. |
ShowDistanceMeasurement | Returns or sets the value indicating if the distance measurement should be displayed. |
Standard | Returns or sets the standard to be used for this ground clearance feature. |
SurfaceLength | Returns or sets the surface length type which determines the length of the general surface. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
UseGeneralSurface | Returns or sets the indication if the general surface will be created. |
UseUnderAxleSurface | Returns or sets the indication if the under axle surface will be created. |
Visualization | Returns or sets the visualization type of the ground clearance output. |
WheelSize | Returns or sets the wheel size definition. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GroundClearanceBuilderPositionType Enumeration | Represents the ground clearance positions. |
GroundClearanceBuilderRequirementControls Enumeration | This enum represents the standard or user defined requirement options for ground clearance. |
GroundClearanceBuilderSectionCurveType Enumeration | Represents the type of under axle section curve type to create ground clearace. |
GroundClearanceBuilderSurfaceLengthType Enumeration | Represents the type of general surface length to create ground clearace. |
GroundClearanceBuilderVisualizationTypes Enumeration | This enum represents the output definition options. |
GroundClearanceBuilderWheelType Enumeration | Represents the type of the wheel size option for ground clearance. |
Property Detail¶
DistanceToRoadGeneral¶
-
GroundClearanceBuilder.
DistanceToRoadGeneral
¶ Returns the expression that contains the value which indicates the distance from general surface to road general.
-------------------------------------
Getter Method
Signature
DistanceToRoadGeneral()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
DistanceToRoadUnderAxle¶
-
GroundClearanceBuilder.
DistanceToRoadUnderAxle
¶ Returns the expression that contains the value which indicates the distance from the under axle surface to road.
-------------------------------------
Getter Method
Signature
DistanceToRoadUnderAxle()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
ExtendSurface¶
-
GroundClearanceBuilder.
ExtendSurface
¶ Returns or sets the indication if use surface extension.
-------------------------------------
Getter Method
Signature
ExtendSurface()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendSurface(extendSurface)
Parameters: extendSurface (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ExtensionFactor¶
-
GroundClearanceBuilder.
ExtensionFactor
¶ Returns the expression that contains the value which indicates the extension factor.
-------------------------------------
Getter Method
Signature
ExtensionFactor()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontUnderAxleFace¶
-
GroundClearanceBuilder.
FrontUnderAxleFace
¶ Returns the faces representing the car body geometry for measuring distance to the front under axle surface.
-------------------------------------
Getter Method
Signature
FrontUnderAxleFace()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
GeneralClearanceFace¶
-
GroundClearanceBuilder.
GeneralClearanceFace
¶ Returns the faces representing the car body geometry for measuring distance to the general surface.
-------------------------------------
Getter Method
Signature
GeneralClearanceFace()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
Loading¶
-
GroundClearanceBuilder.
Loading
¶ Returns or sets the loading to be applied.
Can only be modified when requirements control is
NXOpen.Features.VehicleDesign.GroundClearanceBuilderRequirementControls.UserDefined
.-------------------------------------
Getter Method
Signature
Loading()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Loading(loading)
Parameters: loading (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Position¶
-
GroundClearanceBuilder.
Position
¶ Returns or sets the position of the under axle surface.
-------------------------------------
Getter Method
Signature
Position()
Returns: Return type: NXOpen.Features.VehicleDesign.GroundClearanceBuilderPositionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Position(position)
Parameters: position ( NXOpen.Features.VehicleDesign.GroundClearanceBuilderPositionType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearUnderAxleFace¶
-
GroundClearanceBuilder.
RearUnderAxleFace
¶ Returns the faces representing the car body geometry for measuring distance to the rear under axle surface.
-------------------------------------
Getter Method
Signature
RearUnderAxleFace()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
RequirementsControl¶
-
GroundClearanceBuilder.
RequirementsControl
¶ Returns or sets the value to determine what type of requirement is controlling the ground clearance values.
-------------------------------------
Getter Method
Signature
RequirementsControl()
Returns: Return type: NXOpen.Features.VehicleDesign.GroundClearanceBuilderRequirementControls
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RequirementsControl(requirementsControl)
Parameters: requirementsControl ( NXOpen.Features.VehicleDesign.GroundClearanceBuilderRequirementControls
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SectionCurve¶
-
GroundClearanceBuilder.
SectionCurve
¶ Returns or sets the section curve type of the under axle surface.
See
NXOpen.Features.VehicleDesign.GroundClearanceBuilderSectionCurveType
for valid values.-------------------------------------
Getter Method
Signature
SectionCurve()
Returns: Return type: NXOpen.Features.VehicleDesign.GroundClearanceBuilderSectionCurveType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionCurve(sectionCurveType)
Parameters: sectionCurveType ( NXOpen.Features.VehicleDesign.GroundClearanceBuilderSectionCurveType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowDistanceMeasurement¶
-
GroundClearanceBuilder.
ShowDistanceMeasurement
¶ Returns or sets the value indicating if the distance measurement should be displayed.
-------------------------------------
Getter Method
Signature
ShowDistanceMeasurement()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowDistanceMeasurement(showDistanceMeasurement)
Parameters: showDistanceMeasurement (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Standard¶
-
GroundClearanceBuilder.
Standard
¶ Returns or sets the standard to be used for this ground clearance feature.
Only valid when requirements control is
NXOpen.Features.VehicleDesign.GroundClearanceBuilderRequirementControls.StandardDriven
.-------------------------------------
Getter Method
Signature
Standard()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Standard(standard)
Parameters: standard (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SurfaceLength¶
-
GroundClearanceBuilder.
SurfaceLength
¶ Returns or sets the surface length type which determines the length of the general surface.
See
NXOpen.Features.VehicleDesign.GroundClearanceBuilderSurfaceLengthType
for valid values.-------------------------------------
Getter Method
Signature
SurfaceLength()
Returns: Return type: NXOpen.Features.VehicleDesign.GroundClearanceBuilderSurfaceLengthType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurfaceLength(surfaceLength)
Parameters: surfaceLength ( NXOpen.Features.VehicleDesign.GroundClearanceBuilderSurfaceLengthType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
UseGeneralSurface¶
-
GroundClearanceBuilder.
UseGeneralSurface
¶ Returns or sets the indication if the general surface will be created.
-------------------------------------
Getter Method
Signature
UseGeneralSurface()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseGeneralSurface(useGeneralSurface)
Parameters: useGeneralSurface (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
UseUnderAxleSurface¶
-
GroundClearanceBuilder.
UseUnderAxleSurface
¶ Returns or sets the indication if the under axle surface will be created.
-------------------------------------
Getter Method
Signature
UseUnderAxleSurface()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseUnderAxleSurface(useUnderAxleSurface)
Parameters: useUnderAxleSurface (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Visualization¶
-
GroundClearanceBuilder.
Visualization
¶ Returns or sets the visualization type of the ground clearance output.
-------------------------------------
Getter Method
Signature
Visualization()
Returns: Return type: NXOpen.Features.VehicleDesign.GroundClearanceBuilderVisualizationTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visualization(visualization)
Parameters: visualization ( NXOpen.Features.VehicleDesign.GroundClearanceBuilderVisualizationTypes
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
WheelSize¶
-
GroundClearanceBuilder.
WheelSize
¶ Returns or sets the wheel size definition.
Can only be modified when requirements control is
NXOpen.Features.VehicleDesign.GroundClearanceBuilderRequirementControls.UserDefined
.-------------------------------------
Getter Method
Signature
WheelSize()
Returns: Return type: NXOpen.Features.VehicleDesign.GroundClearanceBuilderWheelType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WheelSize(wheelSize)
Parameters: wheelSize ( NXOpen.Features.VehicleDesign.GroundClearanceBuilderWheelType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
GroundClearanceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.