BumperPendulumBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
BumperPendulumBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.BumperPendulum
builderTo create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateBumperPendulumBuilder()
Default values.
Property Value RequirementsControl StandardDriven Visualization Surface New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
FrontCollector | Returns the selected front body. |
FrontFacetBodies | Returns the selected front facet body |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RearCollector | Returns the selected rear body. |
RearFacetBodies | Returns the selected rear facet body. |
RequirementsControl | Returns or sets the requirements control for standard driven or user defined. |
Standard | Returns or sets the standard used to define the bumper pendulum. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Visualization | Returns or sets the visualization type of the bumper pendulum output. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetPendulum | Get the selected pendulum. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BumperPendulumBuilderRequirementsControlType Enumeration | Represents the requirements control types to define the bumper pendulum. |
BumperPendulumBuilderVisualizationType Enumeration | Represents the visualization types of the output. |
Property Detail¶
FrontCollector¶
-
BumperPendulumBuilder.
FrontCollector
¶ Returns the selected front body.
-------------------------------------
Getter Method
Signature
FrontCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
FrontFacetBodies¶
-
BumperPendulumBuilder.
FrontFacetBodies
¶ Returns the selected front facet body
-------------------------------------
Getter Method
Signature
FrontFacetBodies()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
RearCollector¶
-
BumperPendulumBuilder.
RearCollector
¶ Returns the selected rear body.
-------------------------------------
Getter Method
Signature
RearCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
RearFacetBodies¶
-
BumperPendulumBuilder.
RearFacetBodies
¶ Returns the selected rear facet body.
-------------------------------------
Getter Method
Signature
RearFacetBodies()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
RequirementsControl¶
-
BumperPendulumBuilder.
RequirementsControl
¶ Returns or sets the requirements control for standard driven or user defined.
-------------------------------------
Getter Method
Signature
RequirementsControl()
Returns: Return type: NXOpen.Features.VehicleDesign.BumperPendulumBuilderRequirementsControlType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RequirementsControl(requirement)
Parameters: requirement ( NXOpen.Features.VehicleDesign.BumperPendulumBuilderRequirementsControlType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Standard¶
-
BumperPendulumBuilder.
Standard
¶ Returns or sets the standard used to define the bumper pendulum.
-------------------------------------
Getter Method
Signature
Standard()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Standard(standard)
Parameters: standard (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Visualization¶
-
BumperPendulumBuilder.
Visualization
¶ Returns or sets the visualization type of the bumper pendulum output.
-------------------------------------
Getter Method
Signature
Visualization()
Returns: Return type: NXOpen.Features.VehicleDesign.BumperPendulumBuilderVisualizationType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visualization(visualization)
Parameters: visualization ( NXOpen.Features.VehicleDesign.BumperPendulumBuilderVisualizationType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
GetPendulum¶
-
BumperPendulumBuilder.
GetPendulum
¶ Overloaded method GetPendulum
GetPendulum(index)
GetPendulum(description)
-------------------------------------
Get the selected pendulum.
Signature
GetPendulum(index)
Parameters: index (int) – Returns: Return type: NXOpen.Features.VehicleDesign.PendulumPlacementBuilder
New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
-------------------------------------
Get the selected pendulum.
Signature
GetPendulum(description)
Parameters: description (str) – Returns: Return type: NXOpen.Features.VehicleDesign.PendulumPlacementBuilder
New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
-------------------------------------
Validate¶
-
BumperPendulumBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.