PendulumPlacementBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
PendulumPlacementBuilder
¶ Bases:
NXOpen.Builder
This builder allows you to define the pendulum placement information for bumper pendulum features in vehicle design.
It represents
NXOpen.Features.VehicleDesign.PendulumPlacementBuilder
This class is sub-object of another builder, and cannot be directly instantiated.New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the rotation angle of this pendulum. |
Color | Returns or sets the display color of this pendulum. |
Level | Returns the reference level of this pendulum. |
Loading | Returns or sets the loading used with this pendulum. |
Location | Returns or sets the location to use for positioning this pendulum. |
Name | Returns or sets the name of this pendulum. |
Offset | Returns the side offset of this pendulum. |
PendulumProfile | Returns or sets the pendulum profile of this pendulum. |
PositionMethod | Returns or sets the method to use for positioning this pendulum. |
Shift | Returns the expression containing the amount to shift the pendulum from the contact point on the car. |
ShowPendulum | Returns or sets the value indicating if this pendulum is displayed. |
ShowPoint | Returns or sets the value indicating if the contact point (if any) between this pendulum and the bumper is displayed. |
Side | Returns or sets the side to use for positioning this pendulum. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PendulumPlacementBuilderLocationType Enumeration | This enum represents the pendulum placement location options. |
PendulumPlacementBuilderPendulumProfileType Enumeration | This enum represents the pendulum placement profile options. |
PendulumPlacementBuilderPositionMethodType Enumeration | This enum represents the pendulum placement method options. |
PendulumPlacementBuilderSideType Enumeration | This enum represents the pendulum placement side options. |
Property Detail¶
Angle¶
-
PendulumPlacementBuilder.
Angle
¶ Returns the rotation angle of this pendulum.
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Color¶
-
PendulumPlacementBuilder.
Color
¶ Returns or sets the display color of this pendulum.
-------------------------------------
Getter Method
Signature
Color()
Returns: Return type: Id New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color(color)
Parameters: color (Id) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Level¶
-
PendulumPlacementBuilder.
Level
¶ Returns the reference level of this pendulum.
-------------------------------------
Getter Method
Signature
Level()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Loading¶
-
PendulumPlacementBuilder.
Loading
¶ Returns or sets the loading used with this pendulum.
-------------------------------------
Getter Method
Signature
Loading()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Loading(loading)
Parameters: loading (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Location¶
-
PendulumPlacementBuilder.
Location
¶ Returns or sets the location to use for positioning this pendulum.
-------------------------------------
Getter Method
Signature
Location()
Returns: Return type: NXOpen.Features.VehicleDesign.PendulumPlacementBuilderLocationType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Location(location)
Parameters: location ( NXOpen.Features.VehicleDesign.PendulumPlacementBuilderLocationType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Name¶
-
PendulumPlacementBuilder.
Name
¶ Returns or sets the name of this pendulum.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Offset¶
-
PendulumPlacementBuilder.
Offset
¶ Returns the side offset of this pendulum.
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
PendulumProfile¶
-
PendulumPlacementBuilder.
PendulumProfile
¶ Returns or sets the pendulum profile of this pendulum.
-------------------------------------
Getter Method
Signature
PendulumProfile()
Returns: Return type: NXOpen.Features.VehicleDesign.PendulumPlacementBuilderPendulumProfileType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PendulumProfile(pendulumProfile)
Parameters: pendulumProfile ( NXOpen.Features.VehicleDesign.PendulumPlacementBuilderPendulumProfileType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PositionMethod¶
-
PendulumPlacementBuilder.
PositionMethod
¶ Returns or sets the method to use for positioning this pendulum.
-------------------------------------
Getter Method
Signature
PositionMethod()
Returns: Return type: NXOpen.Features.VehicleDesign.PendulumPlacementBuilderPositionMethodType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PositionMethod(positionMethod)
Parameters: positionMethod ( NXOpen.Features.VehicleDesign.PendulumPlacementBuilderPositionMethodType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Shift¶
-
PendulumPlacementBuilder.
Shift
¶ Returns the expression containing the amount to shift the pendulum from the contact point on the car.
-------------------------------------
Getter Method
Signature
Shift()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
ShowPendulum¶
-
PendulumPlacementBuilder.
ShowPendulum
¶ Returns or sets the value indicating if this pendulum is displayed.
A value of false will hide this pendulum.
-------------------------------------
Getter Method
Signature
ShowPendulum()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowPendulum(showPendulum)
Parameters: showPendulum (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowPoint¶
-
PendulumPlacementBuilder.
ShowPoint
¶ Returns or sets the value indicating if the contact point (if any) between this pendulum and the bumper is displayed.
A value of false will hide the contact point.
-------------------------------------
Getter Method
Signature
ShowPoint()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowPoint(showPoint)
Parameters: showPoint (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Side¶
-
PendulumPlacementBuilder.
Side
¶ Returns or sets the side to use for positioning this pendulum.
-------------------------------------
Getter Method
Signature
Side()
Returns: Return type: NXOpen.Features.VehicleDesign.PendulumPlacementBuilderSideType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side(side)
Parameters: side ( NXOpen.Features.VehicleDesign.PendulumPlacementBuilderSideType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
PendulumPlacementBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.