AllAroundVisionBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
AllAroundVisionBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
A
NXOpen.Features.VehicleDesign.AllAroundVisionBuilder
used to create or edit a vehicle designNXOpen.Features.VehicleDesign.AllAroundVision
feature.To create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateAllAroundVisionBuilder()
Default values.
Property Value CreateIntersectionGeometry 0 UseFrontHeadRests 0 UseRearHeadRests 0 UseWireFrameOnly 0 VisionAreaRadius.Value 0 (millimeters part), 0 (inches part) WindowType Face New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CarGeometry | Returns the faces representing the car geometry to use as obstructing elements. |
CreateIntersectionGeometry | Returns or sets the indication if the intersection geometry should be created. |
DistanceTolerance | Returns or sets the distance tolerance. |
FrontHeadRestGeometry | Returns the faces representing the front head rest geometry to use as obstructing elements. |
ObstructedColor | Returns or sets the color of the obstructed area. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RearHeadRestGeometry | Returns the faces representing the rear head rest geometry to use as obstructing elements. |
SeatReferencePoint | Returns or sets the seat reference point(SgRP). |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Translucency | Returns or sets the translucency of the vision area. |
Type | Returns or sets the type of obstructing geometry being supplied. |
UseFrontHeadRests | Returns or sets the indication if the front head rests geometry should be used. |
UseRearHeadRests | Returns or sets the indication if rear head rests geometry should be used. |
UseWireFrameOnly | Returns or sets the indication if only wire frame should be used. |
VisibleColor | Returns or sets the color of the visible area. |
VisionAreaRadius | Returns the radius of a circle definiing the vision area. |
WindowCurveGeometry | Returns the curves representing the window geometry to use as non-obstructing elements. |
WindowFaceGeometry | Returns the faces representing the window geometry to use as non-obstructing elements. |
WindowType | Returns or sets the type of geometry used to define the window. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AllAroundVisionBuilderTypes Enumeration | Used to indicate the type of obstructing geometry to use. |
AllAroundVisionBuilderWindowTypes Enumeration | Used to indicate the type of geometry used to define the window. |
Property Detail¶
CarGeometry¶
-
AllAroundVisionBuilder.
CarGeometry
¶ Returns the faces representing the car geometry to use as obstructing elements.
-------------------------------------
Getter Method
Signature
CarGeometry()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
CreateIntersectionGeometry¶
-
AllAroundVisionBuilder.
CreateIntersectionGeometry
¶ Returns or sets the indication if the intersection geometry should be created.
-------------------------------------
Getter Method
Signature
CreateIntersectionGeometry()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateIntersectionGeometry(createIntersectionGeometry)
Parameters: createIntersectionGeometry (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
DistanceTolerance¶
-
AllAroundVisionBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance.
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FrontHeadRestGeometry¶
-
AllAroundVisionBuilder.
FrontHeadRestGeometry
¶ Returns the faces representing the front head rest geometry to use as obstructing elements.
-------------------------------------
Getter Method
Signature
FrontHeadRestGeometry()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
ObstructedColor¶
-
AllAroundVisionBuilder.
ObstructedColor
¶ Returns or sets the color of the obstructed area.
-------------------------------------
Getter Method
Signature
ObstructedColor()
Returns: Return type: Id New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ObstructedColor(obstructedColor)
Parameters: obstructedColor (Id) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearHeadRestGeometry¶
-
AllAroundVisionBuilder.
RearHeadRestGeometry
¶ Returns the faces representing the rear head rest geometry to use as obstructing elements.
-------------------------------------
Getter Method
Signature
RearHeadRestGeometry()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
SeatReferencePoint¶
-
AllAroundVisionBuilder.
SeatReferencePoint
¶ Returns or sets the seat reference point(SgRP).
-------------------------------------
Getter Method
Signature
SeatReferencePoint()
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeatReferencePoint(seatReferencePoint)
Parameters: seatReferencePoint ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Translucency¶
-
AllAroundVisionBuilder.
Translucency
¶ Returns or sets the translucency of the vision area.
-------------------------------------
Getter Method
Signature
Translucency()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Translucency(translucency)
Parameters: translucency (int) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Type¶
-
AllAroundVisionBuilder.
Type
¶ Returns or sets the type of obstructing geometry being supplied.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.VehicleDesign.AllAroundVisionBuilderTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.VehicleDesign.AllAroundVisionBuilderTypes
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
UseFrontHeadRests¶
-
AllAroundVisionBuilder.
UseFrontHeadRests
¶ Returns or sets the indication if the front head rests geometry should be used.
-------------------------------------
Getter Method
Signature
UseFrontHeadRests()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseFrontHeadRests(useFrontHeadRests)
Parameters: useFrontHeadRests (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
UseRearHeadRests¶
-
AllAroundVisionBuilder.
UseRearHeadRests
¶ Returns or sets the indication if rear head rests geometry should be used.
-------------------------------------
Getter Method
Signature
UseRearHeadRests()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseRearHeadRests(useRearHeadRests)
Parameters: useRearHeadRests (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
UseWireFrameOnly¶
-
AllAroundVisionBuilder.
UseWireFrameOnly
¶ Returns or sets the indication if only wire frame should be used.
-------------------------------------
Getter Method
Signature
UseWireFrameOnly()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseWireFrameOnly(useWireFrameOnly)
Parameters: useWireFrameOnly (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
VisibleColor¶
-
AllAroundVisionBuilder.
VisibleColor
¶ Returns or sets the color of the visible area.
-------------------------------------
Getter Method
Signature
VisibleColor()
Returns: Return type: Id New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibleColor(visibleColor)
Parameters: visibleColor (Id) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
VisionAreaRadius¶
-
AllAroundVisionBuilder.
VisionAreaRadius
¶ Returns the radius of a circle definiing the vision area.
-------------------------------------
Getter Method
Signature
VisionAreaRadius()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
WindowCurveGeometry¶
-
AllAroundVisionBuilder.
WindowCurveGeometry
¶ Returns the curves representing the window geometry to use as non-obstructing elements.
-------------------------------------
Getter Method
Signature
WindowCurveGeometry()
Returns: Return type: NXOpen.Section
New in version NX8.5.0.
License requirements: None.
WindowFaceGeometry¶
-
AllAroundVisionBuilder.
WindowFaceGeometry
¶ Returns the faces representing the window geometry to use as non-obstructing elements.
-------------------------------------
Getter Method
Signature
WindowFaceGeometry()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
WindowType¶
-
AllAroundVisionBuilder.
WindowType
¶ Returns or sets the type of geometry used to define the window.
-------------------------------------
Getter Method
Signature
WindowType()
Returns: Return type: NXOpen.Features.VehicleDesign.AllAroundVisionBuilderWindowTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WindowType(windowType)
Parameters: windowType ( NXOpen.Features.VehicleDesign.AllAroundVisionBuilderWindowTypes
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
AllAroundVisionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.