AllAroundVisionBuilderTypes Enumeration

NXOpen.Features.VehicleDesign.AllAroundVisionBuilder.Types is an alias for NXOpen.Features.VehicleDesign.AllAroundVisionBuilderTypes

class NXOpen.Features.VehicleDesign.AllAroundVisionBuilderTypes

Bases: object

Used to indicate the type of obstructing geometry to use.

Enum Members

Enum Member Enum Member Description
Pillars
Pillars as obstructing geometry.
Windows
Windows as non-obstructing geometry.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.