AllAroundVisionBuilderWindowTypes Enumeration

NXOpen.Features.VehicleDesign.AllAroundVisionBuilder.WindowTypes is an alias for NXOpen.Features.VehicleDesign.AllAroundVisionBuilderWindowTypes

class NXOpen.Features.VehicleDesign.AllAroundVisionBuilderWindowTypes

Bases: object

Used to indicate the type of geometry used to define the window.

Enum Members

Enum Member Enum Member Description
Face
Face Object for Windows.
Curve
Curve Object for Windows.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.