VisionPlaneBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
VisionPlaneBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.VisionPlane
builder used to create or edit a Vision Plane.To create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateVisionPlaneBuilder()
Default values.
Property Value AssoToggle 1 BaseDim.Value 2000 (millimeters part), 0 (inches part) DriverPlane.Value 4 EyeType EyeFeature FrontDim.Value 1000 (millimeters part), 0 (inches part) FrontPlane.Value 4 LowerPlane 1 MidPlane.Value 1 MiddlePlane 1 PassengerPlane.Value 4 UpperPlane 1 UseStandardLoading 1 VisionType Standard New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AssoToggle | Returns or sets the associative option that determines whether to create feature or not. |
BaseDim | Returns the base dim; dimension from left to right. |
DriverPlane | Returns the driver side plane inclined angle. |
EyeFeature | Returns the eye feature; select eec feature when eye type specified. |
EyeType | Returns or sets the eye type to determine which type of v points to be used. |
FrontDim | Returns the front dim; dimension here to front. |
FrontPlane | Returns the front plane inclined angle. |
LoadingName | Returns or sets the name of the used loading in the Vision Plane. |
LowerPlane | Returns or sets the lower plane option that determines whether to create lower plane or not. |
MidPlane | Returns the middle plane inclined angle; means front side,passenger side and driver side are the same. |
MiddlePlane | Returns or sets the middle plane option that determines whether to create middle plane or not. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PassengerPlane | Returns the passenger side plane inclined angle. |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PointV1 | Returns or sets the point v1; select one point when eye type specified. |
PointV2 | Returns or sets the point v2; select one point when eye type specified. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
UpperPlane | Returns or sets the upper plane option that determines whether to create upper plane or not. |
UseStandardLoading | Returns or sets the option that determines whether to use the loading specified by standard or not. |
VisionType | Returns or sets the vision type; standard or customer defined. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
VisionPlaneBuilderCustomVisionAngle Enumeration | Represents the vision angle type to define the Vision Plane. |
VisionPlaneBuilderEnumEyeType Enumeration | Represents the eye definition type to define the Vision Plane. |
Property Detail¶
AssoToggle¶
-
VisionPlaneBuilder.
AssoToggle
¶ Returns or sets the associative option that determines whether to create feature or not.
-------------------------------------
Getter Method
Signature
AssoToggle()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssoToggle(assoToggle)
Parameters: assoToggle (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
BaseDim¶
-
VisionPlaneBuilder.
BaseDim
¶ Returns the base dim; dimension from left to right.
-------------------------------------
Getter Method
Signature
BaseDim()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
DriverPlane¶
-
VisionPlaneBuilder.
DriverPlane
¶ Returns the driver side plane inclined angle.
-------------------------------------
Getter Method
Signature
DriverPlane()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
EyeFeature¶
-
VisionPlaneBuilder.
EyeFeature
¶ Returns the eye feature; select eec feature when eye type specified.
-------------------------------------
Getter Method
Signature
EyeFeature()
Returns: Return type: NXOpen.Features.SelectFeature
New in version NX6.0.0.
License requirements: None.
EyeType¶
-
VisionPlaneBuilder.
EyeType
¶ Returns or sets the eye type to determine which type of v points to be used.
-------------------------------------
Getter Method
Signature
EyeType()
Returns: Return type: NXOpen.Features.VehicleDesign.VisionPlaneBuilderEnumEyeType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EyeType(eyeType)
Parameters: eyeType ( NXOpen.Features.VehicleDesign.VisionPlaneBuilderEnumEyeType
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FrontDim¶
-
VisionPlaneBuilder.
FrontDim
¶ Returns the front dim; dimension here to front.
-------------------------------------
Getter Method
Signature
FrontDim()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
FrontPlane¶
-
VisionPlaneBuilder.
FrontPlane
¶ Returns the front plane inclined angle.
-------------------------------------
Getter Method
Signature
FrontPlane()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
LoadingName¶
-
VisionPlaneBuilder.
LoadingName
¶ Returns or sets the name of the used loading in the Vision Plane.
-------------------------------------
Getter Method
Signature
LoadingName()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LoadingName(loadingName)
Parameters: loadingName (str) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
LowerPlane¶
-
VisionPlaneBuilder.
LowerPlane
¶ Returns or sets the lower plane option that determines whether to create lower plane or not.
-------------------------------------
Getter Method
Signature
LowerPlane()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowerPlane(lowerPlane)
Parameters: lowerPlane (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
MidPlane¶
-
VisionPlaneBuilder.
MidPlane
¶ Returns the middle plane inclined angle; means front side,passenger side and driver side are the same.
-------------------------------------
Getter Method
Signature
MidPlane()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
MiddlePlane¶
-
VisionPlaneBuilder.
MiddlePlane
¶ Returns or sets the middle plane option that determines whether to create middle plane or not.
-------------------------------------
Getter Method
Signature
MiddlePlane()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MiddlePlane(middlePlane)
Parameters: middlePlane (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PassengerPlane¶
-
VisionPlaneBuilder.
PassengerPlane
¶ Returns the passenger side plane inclined angle.
-------------------------------------
Getter Method
Signature
PassengerPlane()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
PointV1¶
-
VisionPlaneBuilder.
PointV1
¶ Returns or sets the point v1; select one point when eye type specified.
-------------------------------------
Getter Method
Signature
PointV1()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointV1(pointV1)
Parameters: pointV1 ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointV2¶
-
VisionPlaneBuilder.
PointV2
¶ Returns or sets the point v2; select one point when eye type specified.
-------------------------------------
Getter Method
Signature
PointV2()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointV2(pointV2)
Parameters: pointV2 ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
UpperPlane¶
-
VisionPlaneBuilder.
UpperPlane
¶ Returns or sets the upper plane option that determines whether to create upper plane or not.
-------------------------------------
Getter Method
Signature
UpperPlane()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperPlane(upperPlane)
Parameters: upperPlane (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
UseStandardLoading¶
-
VisionPlaneBuilder.
UseStandardLoading
¶ Returns or sets the option that determines whether to use the loading specified by standard or not.
-------------------------------------
Getter Method
Signature
UseStandardLoading()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseStandardLoading(useStandardLoading)
Parameters: useStandardLoading (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
VisionType¶
-
VisionPlaneBuilder.
VisionType
¶ Returns or sets the vision type; standard or customer defined.
-------------------------------------
Getter Method
Signature
VisionType()
Returns: Return type: NXOpen.Features.VehicleDesign.VisionPlaneBuilderCustomVisionAngle
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisionType(visionType)
Parameters: visionType ( NXOpen.Features.VehicleDesign.VisionPlaneBuilderCustomVisionAngle
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
VisionPlaneBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.