VisionPlaneBuilderCustomVisionAngle Enumeration

NXOpen.Features.VehicleDesign.VisionPlaneBuilder.CustomVisionAngle is an alias for NXOpen.Features.VehicleDesign.VisionPlaneBuilderCustomVisionAngle

class NXOpen.Features.VehicleDesign.VisionPlaneBuilderCustomVisionAngle

Bases: object

Represents the vision angle type to define the Vision Plane.

Enum Members

Enum Member Enum Member Description
Standard
standard
Custom
customized
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.