FacetedBodyCollection Class¶
-
class
NXOpen.Facet.
FacetedBodyCollection
¶ Bases:
object
Represents a collection of faceted bodies in a part
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX5.0.0.
“FacetModelingCollection”, ” Returns the FacetModelingCollection instance belonging to this part “
Methods¶
Enumerations¶
FacetedBodyCollectionType Enumeration | Specifies the type of facets created when copying or converting faceted bodies |
FacetModelingCollection¶
-
FacetedBodyCollection.
FacetModelingCollection
¶ Returns the FacetModelingCollection instance belonging to this part
Signature
FacetModelingCollection()
New in version NX10.0.0.
Returns: Return type: NXOpen.Facet.FacetModelingCollection
Method Detail¶
Convert¶
-
FacetedBodyCollection.
Convert
¶ Converts the internal representation of this faceted body to the specified type.
This does not create a new body
Signature
Convert(fromBody, toFacetType)
Parameters: - fromBody (
NXOpen.Facet.FacetedBody
) – The faceted body to convert - toFacetType (
NXOpen.Facet.FacetedBodyCollectionType
) – To facet type
New in version NX5.0.0.
License requirements: None.
- fromBody (
Copy¶
-
FacetedBodyCollection.
Copy
¶ Copies a faceted body and optionally changes the internal representation to the given type (This is only valid for JT to NX copy)
Signature
Copy(fromBody, toPart, toFacetType)
Parameters: - fromBody (
NXOpen.Facet.FacetedBody
) – The faceted body to copy - toPart (
NXOpen.Part
) – Part to create the copy in - toFacetType (
NXOpen.Facet.FacetedBodyCollectionType
) – To facet type
Returns: New body
Return type: New in version NX5.0.0.
License requirements: None.
- fromBody (
CreateBestFitAlignBuilder¶
-
FacetedBodyCollection.
CreateBestFitAlignBuilder
¶ Creates a
NXOpen.Facet.BestFitAlignBuilder
Signature
CreateBestFitAlignBuilder()
Returns: Return type: NXOpen.Facet.BestFitAlignBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_1 (“basic freeform modeling”)
CreateBridgeFacetBodyBuilder¶
-
FacetedBodyCollection.
CreateBridgeFacetBodyBuilder
¶ Creates a
NXOpen.Facet.BridgeFacetBodyBuilder
Signature
CreateBridgeFacetBodyBuilder()
Returns: Return type: NXOpen.Facet.BridgeFacetBodyBuilder
New in version NX9.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”) OR die_engineering (“DIE ENGINEERING”)
CreateDecimateFacetBodyBuilder¶
-
FacetedBodyCollection.
CreateDecimateFacetBodyBuilder
¶ Creates a
NXOpen.Facet.DecimateFacetBodyBuilder
Signature
CreateDecimateFacetBodyBuilder()
Returns: Return type: NXOpen.Facet.DecimateFacetBodyBuilder
New in version NX7.5.0.
License requirements: nx_freeform_1 (“basic freeform modeling”)
CreateExtrudeFacetBodyBuilder¶
-
FacetedBodyCollection.
CreateExtrudeFacetBodyBuilder
¶ Creates a
NXOpen.Facet.ExtrudeFacetBodyBuilder
Signature
CreateExtrudeFacetBodyBuilder()
Returns: Return type: NXOpen.Facet.ExtrudeFacetBodyBuilder
New in version NX9.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”) OR die_engineering (“DIE ENGINEERING”)
CreateExtrudeProfileBuilder¶
-
FacetedBodyCollection.
CreateExtrudeProfileBuilder
¶ Creates a
NXOpen.Facet.ExtrudeProfileBuilder
Signature
CreateExtrudeProfileBuilder()
Returns: Return type: NXOpen.Facet.ExtrudeProfileBuilder
New in version NX9.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”) OR die_engineering (“DIE ENGINEERING”)
CreateFacetBody¶
-
FacetedBodyCollection.
CreateFacetBody
¶ Creates a JT
NXOpen.Facet.FacetedBody
using the default faceting tolerances.The output facetBodies and errorTable arrays are the same size as the input nSolidBodies. The errorTable array provides information about any errors encountered when faceting bodies. Note that it is possible that faceted bodies with 0 facets are created (and returned in the facetBodies parameter). For this case, the errorTable will contain the UF_FACET_err_zero_facets_produced error. If there is an existing facet body it will get refaceted with the previous tolerance used to tessellate it . See
NXOpen.Body.GetFacetedBody()
for ways to check for this situation.Signature
CreateFacetBody(solidBodies)
Parameters: solidBodies (list of NXOpen.Body
) –Returns: a tuple Return type: A tuple consisting of (facetBodies, errorTable). facetBodies is a list of NXOpen.Facet.FacetedBody
. errorTable is a list of int.New in version NX7.5.5.
License requirements: adv_assemblies (“ADVANCED ASSEMBLIES”)
CreateFacetBodyFromFaces¶
-
FacetedBodyCollection.
CreateFacetBodyFromFaces
¶ Creates a JT
NXOpen.Facet.FacetedBody
using the default faceting tolerances.The output facetBodies and errorTable arrays are the same size as the input nSolidFaces. The errorTable array provides information about any errors encountered when faceting bodies. Note that it is possible that faceted bodies with 0 facets are created (and returned in the facetBodies parameter). For this case, the errorTable will contain the UF_FACET_err_zero_facets_produced error. If there is an existing facet body it will get refaceted with the previous tolerance used to tessellate it . See
NXOpen.Body.GetFacetedBody()
for ways to check for this situation.Signature
CreateFacetBodyFromFaces(solidFaces)
Parameters: solidFaces (list of NXOpen.Face
) –Returns: a tuple Return type: A tuple consisting of (facetBodies, errorTable). facetBodies is a list of NXOpen.Facet.FacetedBody
. errorTable is a list of int.New in version NX8.5.0.
License requirements: adv_assemblies (“ADVANCED ASSEMBLIES”)
CreateFacetCurvatureBuilder¶
-
FacetedBodyCollection.
CreateFacetCurvatureBuilder
¶ Create a
NXOpen.Facet.CurvatureBuilder
object.Signature
CreateFacetCurvatureBuilder()
Returns: Return type: NXOpen.Facet.CurvatureBuilder
New in version NX5.0.0.
License requirements: None.
CreateFacetFeatureExtractionBuilder¶
-
FacetedBodyCollection.
CreateFacetFeatureExtractionBuilder
¶ Create a
NXOpen.Facet.FeatureExtractionBuilder
object.Signature
CreateFacetFeatureExtractionBuilder()
Returns: Return type: NXOpen.Facet.FeatureExtractionBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CreateFillHoleBuilder¶
-
FacetedBodyCollection.
CreateFillHoleBuilder
¶ Creates a
NXOpen.Facet.FillHoleBuilder
Signature
CreateFillHoleBuilder()
Returns: Return type: NXOpen.Facet.FillHoleBuilder
New in version NX6.0.0.
License requirements: None.
CreateMergeFacetBodyBuilder¶
-
FacetedBodyCollection.
CreateMergeFacetBodyBuilder
¶ Creates a
NXOpen.Facet.MergeFacetBodyBuilder
Signature
CreateMergeFacetBodyBuilder()
Returns: Return type: NXOpen.Facet.MergeFacetBodyBuilder
New in version NX9.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”) OR die_engineering (“DIE ENGINEERING”)
CreateMultiPatchAlignmentBuilder¶
-
FacetedBodyCollection.
CreateMultiPatchAlignmentBuilder
¶ Creates a
NXOpen.Facet.MultiPatchAlignmentBuilder
Signature
CreateMultiPatchAlignmentBuilder()
Returns: Return type: NXOpen.Facet.MultiPatchAlignmentBuilder
New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CreateSTLImportBuilder¶
-
FacetedBodyCollection.
CreateSTLImportBuilder
¶ Creates a
NXOpen.Facet.STLImportBuilder
Signature
CreateSTLImportBuilder()
Returns: Return type: NXOpen.Facet.STLImportBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_1 (“basic freeform modeling”)
CreateSewFacetBodyBuilder¶
-
FacetedBodyCollection.
CreateSewFacetBodyBuilder
¶ Creates a
NXOpen.Facet.SewFacetBodyBuilder
Signature
CreateSewFacetBodyBuilder()
Returns: Return type: NXOpen.Facet.SewFacetBodyBuilder
New in version NX9.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”) OR die_engineering (“DIE ENGINEERING”)
CreateSmoothFacetBodyBuilder¶
-
FacetedBodyCollection.
CreateSmoothFacetBodyBuilder
¶ Creates a
NXOpen.Facet.SmoothFacetBodyBuilder
Signature
CreateSmoothFacetBodyBuilder()
Returns: Return type: NXOpen.Facet.SmoothFacetBodyBuilder
New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CreateSnipFacetBodyBuilder¶
-
FacetedBodyCollection.
CreateSnipFacetBodyBuilder
¶ Creates a
NXOpen.Facet.SnipFacetBodyBuilder
Signature
CreateSnipFacetBodyBuilder()
Returns: Return type: NXOpen.Facet.SnipFacetBodyBuilder
New in version NX6.0.0.
License requirements: None.
CreateSubdivideFacetBodyBuilder¶
-
FacetedBodyCollection.
CreateSubdivideFacetBodyBuilder
¶ Creates a
NXOpen.Facet.SubdivideFacetBodyBuilder
Signature
CreateSubdivideFacetBodyBuilder()
Returns: Return type: NXOpen.Facet.SubdivideFacetBodyBuilder
New in version NX7.5.0.
License requirements: nx_freeform_1 (“basic freeform modeling”)
DeleteTemporaryFacesAndEdges¶
-
FacetedBodyCollection.
DeleteTemporaryFacesAndEdges
¶ Delete any temporary faces and edges on faceted bodies that may have been created in the specified part.
Please note that this call will invoke an Update operation.
Signature
DeleteTemporaryFacesAndEdges()
New in version NX5.0.2.
License requirements: None.
FindObject¶
-
FacetedBodyCollection.
FindObject
¶ Finds the
NXOpen.Facet.FacetedBody
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the faceted body you want Returns: Faceted body with this identifier Return type: NXOpen.Facet.FacetedBody
New in version NX5.0.0.
License requirements: None.
GetAssociatedFacetedBodies¶
-
FacetedBodyCollection.
GetAssociatedFacetedBodies
¶ Returns the loaded solid bodies associated with the argument faceted body.
Also returns the number of unloaded associated faceted bodies.
Signature
GetAssociatedFacetedBodies(solidBody)
Parameters: solidBody ( NXOpen.Body
) – The body for which to get associated faceted bodiesReturns: a tuple Return type: A tuple consisting of (associatedFacetedBodies, numberOfUnloadedFacetedBodies). associatedFacetedBodies is a list of NXOpen.Facet.FacetedBody
. Array of loaded associated faceted bodies numberOfUnloadedFacetedBodies is a int. The number of unloaded associated faceted bodies for this solids bodyNew in version NX5.0.0.
License requirements: None.