CurvatureBuilder Class¶
-
class
NXOpen.Facet.
CurvatureBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Facet.CurvatureBuilder
.It calculates the maximum absolute principal curvature on facet bodies and creates a color map of these values.
To create a new instance of this class, use
NXOpen.Facet.FacetedBodyCollection.CreateFacetCurvatureBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Bodies | Returns the input facet body list. |
ConcaveRadius | Returns or sets the concave radius threshold |
ConvexRadius | Returns or sets the convex radius threshold |
FacetBodies | Returns the input facet body list |
IsDirectionReversed | Returns or sets the reverse direction option |
SmoothingFactor | Returns or sets the smoothing factor |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
DeleteCurvature | Deletes the curvature data associated with the input facet bodies. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Bodies¶
-
CurvatureBuilder.
Bodies
¶ Returns the input facet body list.
Inputs to this command can be convergent objects.
-------------------------------------
Getter Method
Signature
Bodies()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX11.0.0.
License requirements: None.
ConcaveRadius¶
-
CurvatureBuilder.
ConcaveRadius
¶ Returns or sets the concave radius threshold
-------------------------------------
Getter Method
Signature
ConcaveRadius()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConcaveRadius(concaveRadius)
Parameters: concaveRadius (float) – New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ConvexRadius¶
-
CurvatureBuilder.
ConvexRadius
¶ Returns or sets the convex radius threshold
-------------------------------------
Getter Method
Signature
ConvexRadius()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConvexRadius(convexRadius)
Parameters: convexRadius (float) – New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
FacetBodies¶
-
CurvatureBuilder.
FacetBodies
¶ Returns the input facet body list
-------------------------------------
Getter Method
Signature
FacetBodies()
Returns: Return type: NXOpen.Facet.SelectFacetedBodyList
New in version NX5.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Facet.CurvatureBuilder.Bodies()
instead.License requirements: None.
IsDirectionReversed¶
-
CurvatureBuilder.
IsDirectionReversed
¶ Returns or sets the reverse direction option
-------------------------------------
Getter Method
Signature
IsDirectionReversed()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsDirectionReversed(directionReversed)
Parameters: directionReversed (bool) – New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SmoothingFactor¶
-
CurvatureBuilder.
SmoothingFactor
¶ Returns or sets the smoothing factor
-------------------------------------
Getter Method
Signature
SmoothingFactor()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmoothingFactor(smoothingFactor)
Parameters: smoothingFactor (float) – New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
DeleteCurvature¶
-
CurvatureBuilder.
DeleteCurvature
¶ Deletes the curvature data associated with the input facet bodies.
Call this method in order to save memory if the curvature data are not needed any more.
Signature
DeleteCurvature()
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Validate¶
-
CurvatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.