FeatureExtractionBuilder Class¶
-
class
NXOpen.Facet.
FeatureExtractionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Facet.FeatureExtractionBuilder
It extracts feature lines or separates regions of different curvature from a facet body based on the curvature map.For facet body curvature, please see
NXOpen.Facet.CurvatureBuilder
.To create a new instance of this class, use
NXOpen.Facet.FacetedBodyCollection.CreateFacetFeatureExtractionBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AreBordersEnabled | Returns or sets the extracting borders option |
AreRegionsEnabled | Returns or sets the extracting regions option |
FacetBodies | Returns the input facet body selection list |
InputAction | Returns or sets the input facet body action |
IsSmoothingEnabled | Returns or sets the smoothing option |
MinimumBorderLength | Returns or sets the minimum border length |
SmoothingFactor | Returns or sets the smoothing factor |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetExtractedBorders | Gets the extracted curves. |
GetExtractedRegions | Gets the extracted facet bodies. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FeatureExtractionBuilderInputActions Enumeration | Specifies how to handle the input facet bodies. |
Property Detail¶
AreBordersEnabled¶
-
FeatureExtractionBuilder.
AreBordersEnabled
¶ Returns or sets the extracting borders option
-------------------------------------
Getter Method
Signature
AreBordersEnabled()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AreBordersEnabled(bordersEnabled)
Parameters: bordersEnabled (bool) – New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
AreRegionsEnabled¶
-
FeatureExtractionBuilder.
AreRegionsEnabled
¶ Returns or sets the extracting regions option
-------------------------------------
Getter Method
Signature
AreRegionsEnabled()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AreRegionsEnabled(regionsEnabled)
Parameters: regionsEnabled (bool) – New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
FacetBodies¶
-
FeatureExtractionBuilder.
FacetBodies
¶ Returns the input facet body selection list
-------------------------------------
Getter Method
Signature
FacetBodies()
Returns: Return type: NXOpen.Facet.SelectFacetedBodyList
New in version NX5.0.0.
License requirements: None.
InputAction¶
-
FeatureExtractionBuilder.
InputAction
¶ Returns or sets the input facet body action
-------------------------------------
Getter Method
Signature
InputAction()
Returns: Return type: NXOpen.Facet.FeatureExtractionBuilderInputActions
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InputAction(inputAction)
Parameters: inputAction ( NXOpen.Facet.FeatureExtractionBuilderInputActions
) –New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
IsSmoothingEnabled¶
-
FeatureExtractionBuilder.
IsSmoothingEnabled
¶ Returns or sets the smoothing option
-------------------------------------
Getter Method
Signature
IsSmoothingEnabled()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSmoothingEnabled(smoothingEanbled)
Parameters: smoothingEanbled (bool) – New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
MinimumBorderLength¶
-
FeatureExtractionBuilder.
MinimumBorderLength
¶ Returns or sets the minimum border length
-------------------------------------
Getter Method
Signature
MinimumBorderLength()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumBorderLength(minimumBorderLength)
Parameters: minimumBorderLength (float) – New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SmoothingFactor¶
-
FeatureExtractionBuilder.
SmoothingFactor
¶ Returns or sets the smoothing factor
-------------------------------------
Getter Method
Signature
SmoothingFactor()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmoothingFactor(smoothingFactor)
Parameters: smoothingFactor (float) – New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
GetExtractedBorders¶
-
FeatureExtractionBuilder.
GetExtractedBorders
¶ Gets the extracted curves.
Call
Builder.Commit()
before calling this method.Signature
GetExtractedBorders()
Returns: The extracted curves Return type: list of NXOpen.Spline
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
GetExtractedRegions¶
-
FeatureExtractionBuilder.
GetExtractedRegions
¶ Gets the extracted facet bodies.
Call
Builder.Commit()
before calling this method.Signature
GetExtractedRegions()
Returns: The extracted facet bodies Return type: list of NXOpen.Facet.FacetedBody
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Validate¶
-
FeatureExtractionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.