FacetedBody Class¶
-
class
NXOpen.Facet.
FacetedBody
¶ Bases:
NXOpen.DisplayableObject
Represents a faceted body.
Instances of this class cannot be created directly by the user, but can be created using the methods of FacetedBodyCollection.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AssociatedBody | Returns the solid body associated with this facet body. |
BodyType | Returns the type of the body |
Color | Returns or sets the color of the object. |
IsAssemblyLevel | Returns a flag indicating this is an assembly level representation. |
IsAssociatedBodyLoaded | Returns the load state of the solid body associated with this facet body. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsSheetBody | Returns true if the body is a sheet body |
IsSolidBody | Returns true if the body is a solid body |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
NumberOfFaces | Returns the number of faces in this faceted body in the highest level of detail. |
NumberOfLevelsOfDetail | Returns the number of levels of detail in this faceted body. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
SurfaceArea | Returns the surface area of the faceted body in part units for its highest level of detail. |
Tag | Returns the Tag for this object. |
Volume | Returns the volume of the faceted body in part units for its highest level of detail. |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetEdges | Returns the edges in the faceted body @return |
GetFaces | Returns the faces in the faceted body @return |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetNumberOfEdges | Returns the number of edges in the faceted body @return |
GetNumberOfFacets | Get the number of facets in the given level of detail. |
GetParameters | Get the faceted body parameters @return faceting parameters for this body |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasLightWeightAnalytics | Returns whether the FACET has analytical information @return |
HasTopologyInformation | Returns whether the FACET has topology information @return |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Highlight | Highlights the object. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveViewDependency | Remove dependency on all views from an object. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetParameters | Set the faceted body parameters, it will retessellate the body with the new parameters |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Enumerations¶
FacetedBodyFacetedbodyType Enumeration | Body type |
Property Detail¶
AssociatedBody¶
-
FacetedBody.
AssociatedBody
¶ Returns the solid body associated with this facet body.
-------------------------------------
Getter Method
Signature
AssociatedBody()
Returns: Return type: NXOpen.Body
New in version NX5.0.0.
License requirements: None.
BodyType¶
-
FacetedBody.
BodyType
¶ Returns the type of the body
-------------------------------------
Getter Method
Signature
BodyType()
Returns: Return type: NXOpen.Facet.FacetedBodyFacetedbodyType
New in version NX8.5.1.
License requirements: None.
IsAssemblyLevel¶
-
FacetedBody.
IsAssemblyLevel
¶ Returns a flag indicating this is an assembly level representation.
That is this facet body is associated with an occurrence of a solid body.
-------------------------------------
Getter Method
Signature
IsAssemblyLevel()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
IsAssociatedBodyLoaded¶
-
FacetedBody.
IsAssociatedBodyLoaded
¶ Returns the load state of the solid body associated with this facet body.
False if there is no associated body.
-------------------------------------
Getter Method
Signature
IsAssociatedBodyLoaded()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
IsOccurrence¶
-
FacetedBody.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
IsSheetBody¶
-
FacetedBody.
IsSheetBody
¶ Returns true if the body is a sheet body
-------------------------------------
Getter Method
Signature
IsSheetBody()
Returns: Return type: bool New in version NX5.0.0.
Deprecated since version NX8.5.1: Use
NXOpen.Facet.FacetedBody.BodyType()
insteadLicense requirements: None.
IsSolidBody¶
-
FacetedBody.
IsSolidBody
¶ Returns true if the body is a solid body
-------------------------------------
Getter Method
Signature
IsSolidBody()
Returns: Return type: bool New in version NX5.0.0.
Deprecated since version NX8.5.1: Use
NXOpen.Facet.FacetedBody.BodyType()
instead.License requirements: None.
JournalIdentifier¶
-
FacetedBody.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
FacetedBody.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
NumberOfFaces¶
-
FacetedBody.
NumberOfFaces
¶ Returns the number of faces in this faceted body in the highest level of detail.
-------------------------------------
Getter Method
Signature
NumberOfFaces()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
NumberOfLevelsOfDetail¶
-
FacetedBody.
NumberOfLevelsOfDetail
¶ Returns the number of levels of detail in this faceted body.
-------------------------------------
Getter Method
Signature
NumberOfLevelsOfDetail()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
OwningComponent¶
-
FacetedBody.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
FacetedBody.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
FacetedBody.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
FacetedBody.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetEdges¶
-
FacetedBody.
GetEdges
¶ Returns the edges in the faceted body
Signature
GetEdges()
Returns: Return type: list of NXOpen.Facet.FacetedEdge
New in version NX8.5.1.
License requirements: None.
GetFaces¶
-
FacetedBody.
GetFaces
¶ Returns the faces in the faceted body
Signature
GetFaces()
Returns: Return type: list of NXOpen.Facet.FacetedFace
New in version NX8.5.1.
License requirements: None.
GetNumberOfEdges¶
-
FacetedBody.
GetNumberOfEdges
¶ Returns the number of edges in the faceted body
Signature
GetNumberOfEdges()
Returns: Return type: int New in version NX8.5.1.
License requirements: None.
GetNumberOfFacets¶
-
FacetedBody.
GetNumberOfFacets
¶ Get the number of facets in the given level of detail.
Signature
GetNumberOfFacets(levelOfDetail)
Parameters: levelOfDetail (int) – level of detail to query Returns: Return type: int New in version NX5.0.0.
License requirements: None.
GetParameters¶
-
FacetedBody.
GetParameters
¶ Get the faceted body parameters
Signature
GetParameters()
Returns: faceting parameters for this body Return type: NXOpen.Facet.FacetingParameters
New in version NX5.0.0.
License requirements: None.
HasLightWeightAnalytics¶
-
FacetedBody.
HasLightWeightAnalytics
¶ Returns whether the FACET has analytical information
Signature
HasLightWeightAnalytics()
Returns: Return type: bool New in version NX8.5.1.
License requirements: None.
HasTopologyInformation¶
-
FacetedBody.
HasTopologyInformation
¶ Returns whether the FACET has topology information
Signature
HasTopologyInformation()
Returns: Return type: bool New in version NX8.5.1.
License requirements: None.
Print¶
-
FacetedBody.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
FacetedBody.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetParameters¶
-
FacetedBody.
SetParameters
¶ Set the faceted body parameters, it will retessellate the body with the new parameters
Signature
SetParameters(parameters)
Parameters: parameters ( NXOpen.Facet.FacetingParameters
) – new facetting faceting parameters to set for this bodyNew in version NX5.0.0.
License requirements: None.