BridgeFacetBodyBuilder Class¶
-
class
NXOpen.Facet.
BridgeFacetBodyBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Facet.BridgeFacetBodyBuilder
It bridges two disjoint NX facet bodies.User need to specify the range for each input facet body. It returns a new megered NX facet Body. The two input bodies can be kept, deleted or hidden.
To create a new instance of this class, use
NXOpen.Facet.FacetedBodyCollection.CreateBridgeFacetBodyBuilder()
Default values.
Property Value InputStatus Keep Smoothness Linear New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
DistanceTolerance | Returns or sets the distance tolerance used in the bridge facet body feature |
FacetBodyOne | Returns the first NX facet body to be bridged |
FacetBodyTwo | Returns the second NX facet body to be bridged |
InputStatus | Returns or sets the option to specify how to deal with the input two facet bodies: keep, delete or hide |
Smoothness | Returns or sets the inserted facet smooth type |
Tag | Returns the Tag for this object. |
Vertex1Range1 | Returns or sets the first vertex used to define the range on the the first facet body |
Vertex1Range2 | Returns or sets the first vertex used to defind the range on the second facet body |
Vertex2Range1 | Returns or sets the second vertex used to define the range on the first facet body |
Vertex2Range2 | Returns or sets the second vertex used to defind the range on the second facet body |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FlipRange1 | Flip the range between the first and second vertex on the first facet body |
FlipRange2 | Flip the range between the first and second vertex on the second facet body |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BridgeFacetBodyBuilderInput Enumeration | Represents the option for keeping, deleting or hiding input two facet bodies after builder committing |
BridgeFacetBodyBuilderSmoothTypes Enumeration | Represents the smoothness type for the inserted new facets |
Property Detail¶
DistanceTolerance¶
-
BridgeFacetBodyBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance used in the bridge facet body feature
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX9.0.2.
License requirements: None.
FacetBodyOne¶
-
BridgeFacetBodyBuilder.
FacetBodyOne
¶ Returns the first NX facet body to be bridged
-------------------------------------
Getter Method
Signature
FacetBodyOne()
Returns: Return type: NXOpen.Facet.SelectFacetedBody
New in version NX9.0.0.
License requirements: None.
FacetBodyTwo¶
-
BridgeFacetBodyBuilder.
FacetBodyTwo
¶ Returns the second NX facet body to be bridged
-------------------------------------
Getter Method
Signature
FacetBodyTwo()
Returns: Return type: NXOpen.Facet.SelectFacetedBody
New in version NX9.0.0.
License requirements: None.
InputStatus¶
-
BridgeFacetBodyBuilder.
InputStatus
¶ Returns or sets the option to specify how to deal with the input two facet bodies: keep, delete or hide
-------------------------------------
Getter Method
Signature
InputStatus()
Returns: Return type: NXOpen.Facet.BridgeFacetBodyBuilderInput
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InputStatus(inputStatus)
Parameters: inputStatus ( NXOpen.Facet.BridgeFacetBodyBuilderInput
) –New in version NX9.0.0.
License requirements: None.
Smoothness¶
-
BridgeFacetBodyBuilder.
Smoothness
¶ Returns or sets the inserted facet smooth type
-------------------------------------
Getter Method
Signature
Smoothness()
Returns: Return type: NXOpen.Facet.BridgeFacetBodyBuilderSmoothTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Smoothness(smoothType)
Parameters: smoothType ( NXOpen.Facet.BridgeFacetBodyBuilderSmoothTypes
) –New in version NX9.0.0.
License requirements: None.
Vertex1Range1¶
-
BridgeFacetBodyBuilder.
Vertex1Range1
¶ Returns or sets the first vertex used to define the range on the the first facet body
-------------------------------------
Getter Method
Signature
Vertex1Range1()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vertex1Range1(vertex1Range1)
Parameters: vertex1Range1 ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: None.
Vertex1Range2¶
-
BridgeFacetBodyBuilder.
Vertex1Range2
¶ Returns or sets the first vertex used to defind the range on the second facet body
-------------------------------------
Getter Method
Signature
Vertex1Range2()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vertex1Range2(vertex1Range2)
Parameters: vertex1Range2 ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: None.
Vertex2Range1¶
-
BridgeFacetBodyBuilder.
Vertex2Range1
¶ Returns or sets the second vertex used to define the range on the first facet body
-------------------------------------
Getter Method
Signature
Vertex2Range1()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vertex2Range1(vertex2Range1)
Parameters: vertex2Range1 ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: None.
Vertex2Range2¶
-
BridgeFacetBodyBuilder.
Vertex2Range2
¶ Returns or sets the second vertex used to defind the range on the second facet body
-------------------------------------
Getter Method
Signature
Vertex2Range2()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vertex2Range2(vertex2Range2)
Parameters: vertex2Range2 ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: None.
Method Detail¶
FlipRange1¶
-
BridgeFacetBodyBuilder.
FlipRange1
¶ Flip the range between the first and second vertex on the first facet body
Signature
FlipRange1()
New in version NX9.0.0.
License requirements: None.
FlipRange2¶
-
BridgeFacetBodyBuilder.
FlipRange2
¶ Flip the range between the first and second vertex on the second facet body
Signature
FlipRange2()
New in version NX9.0.0.
License requirements: None.
Validate¶
-
BridgeFacetBodyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.