BridgeFacetBodyBuilderSmoothTypes Enumeration

NXOpen.Facet.BridgeFacetBodyBuilder.SmoothTypes is an alias for NXOpen.Facet.BridgeFacetBodyBuilderSmoothTypes

class NXOpen.Facet.BridgeFacetBodyBuilderSmoothTypes

Bases: object

Represents the smoothness type for the inserted new facets

Enum Members

Enum Member Enum Member Description
Linear
Insert new facets with linear smoothness
TangentBased
Insert new facets with tangent smoothness
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.