MultiPatchAlignmentBuilder Class¶
-
class
NXOpen.Facet.
MultiPatchAlignmentBuilder
¶ Bases:
NXOpen.Builder
Aligns multiple facet bodies to one another without using reference points.
To create a new instance of this class, use
NXOpen.Facet.FacetedBodyCollection.CreateMultiPatchAlignmentBuilder()
Default values.
Property Value Iteration 10 MaximumCheckingDistance 10.0 (millimeters part), 0.5 (inches part) Resolution High Tolerance 0.01 (millimeters part), 0.005 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AlignmentBodies | Returns the facet bodies to be aligned. |
Iteration | Returns or sets the value indicating the number of times the alignment algorithm is applied. |
MaximumCheckingDistance | Returns or sets the distance facets may be from one another in order to be used in the alignment. |
ReferencePatches | Returns an optional reference facet body with a location and orientation that will remain fixed, causing all of the other selected facet bodies to align with it. |
Resolution | Returns or sets the type indicating number of facets to be used in the alignment. |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the precision of the alignment. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MultiPatchAlignmentBuilderResolutionType Enumeration | Determines the number of facets used in the alignment. |
Property Detail¶
AlignmentBodies¶
-
MultiPatchAlignmentBuilder.
AlignmentBodies
¶ Returns the facet bodies to be aligned.
-------------------------------------
Getter Method
Signature
AlignmentBodies()
Returns: Return type: NXOpen.Facet.SelectFacetedBodyList
New in version NX7.5.0.
License requirements: None.
Iteration¶
-
MultiPatchAlignmentBuilder.
Iteration
¶ Returns or sets the value indicating the number of times the alignment algorithm is applied.
Many iterations improve alignment accuracy but take longer.
-------------------------------------
Getter Method
Signature
Iteration()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Iteration(iteration)
Parameters: iteration (int) – New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
MaximumCheckingDistance¶
-
MultiPatchAlignmentBuilder.
MaximumCheckingDistance
¶ Returns or sets the distance facets may be from one another in order to be used in the alignment.
Larger numbers slow the alignment process.
-------------------------------------
Getter Method
Signature
MaximumCheckingDistance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumCheckingDistance(maximumCheckingDistance)
Parameters: maximumCheckingDistance (float) – New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ReferencePatches¶
-
MultiPatchAlignmentBuilder.
ReferencePatches
¶ Returns an optional reference facet body with a location and orientation that will remain fixed, causing all of the other selected facet bodies to align with it.
If you do not select a reference body, all of the selected facet bodies will align to each other, without a fixed location.
-------------------------------------
Getter Method
Signature
ReferencePatches()
Returns: Return type: NXOpen.Facet.SelectFacetedBodyList
New in version NX7.5.0.
License requirements: None.
Resolution¶
-
MultiPatchAlignmentBuilder.
Resolution
¶ Returns or sets the type indicating number of facets to be used in the alignment.
-------------------------------------
Getter Method
Signature
Resolution()
Returns: Return type: NXOpen.Facet.MultiPatchAlignmentBuilderResolutionType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Resolution(resolution)
Parameters: resolution ( NXOpen.Facet.MultiPatchAlignmentBuilderResolutionType
) –New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Tolerance¶
-
MultiPatchAlignmentBuilder.
Tolerance
¶ Returns or sets the precision of the alignment.
Alignment will complete when tolerance is met or the number of iterations has been reached.
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
Validate¶
-
MultiPatchAlignmentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.