InspectionScanHelixBuilder Class¶
-
class
NXOpen.CAM.
InspectionScanHelixBuilder
¶ Bases:
NXOpen.CAM.InspectionMoveBuilder
Represents the builder for the CMM Inspection sub-operation Scan Helix.
To create a new instance of this class, use
NXOpen.CAM.InspectionMoveCollection.CreateInspectionScanHelixBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AngleA | Returns or sets the A angle for an indexable head |
AngleB | Returns or sets the B angle for an indexable head |
ApproachDist | Returns the builder for approach distance |
ApproachDistance | Returns or sets the approach distance |
DepthDistance | Returns or sets the depth distance |
DepthMethod | Returns or sets the depth method |
EndDistance | Returns the End Distance of the Scan Helix |
EndPercentage | Returns the End Percentage of the Scan Helix |
MotionType | Returns or sets the motion type |
Pitch | Returns the pitch of the Scan Helix |
ProbeTipType | Returns or sets the preferred probe tip type |
ProbeTipTypeBuilder | Returns the Probe Tip Type Builder |
RetractDist | Returns the builder for retract distance |
RetractDistance | Returns or sets the retract distance |
Reversedirection | Returns or sets the Reverse Direction flag on the Helix |
Revolutions | Returns the revolutions of the Scan Helix |
ScanModeType | Returns or sets the 3,5 axis mode type |
ScanSpeed | Returns the builder for scan speed |
SensorOpName | Returns or sets the inspection sensor operation name |
SensorStrategy | Returns or sets the sensor selection strategy |
SensorStrategyBuilder | Returns the Sensor Strategy Enum Builder |
StartDistance | Returns the Start Distance of the Scan Helix |
StartEndMode | Returns or sets the start/end mode |
StartPercentage | Returns the Start Percentage of the Scan Helix |
StepSize | Returns the builder for step size |
Sweep | Returns the sweep of the Scan Helix |
Tag | Returns the Tag for this object. |
TipAngleMode | Returns or sets the tip angle selection mode |
TipMode | Returns or sets the probe tip selection mode |
TipNumber | Returns or sets the probe tip number |
TurnDirection | Returns or sets the turn direction type |
TurnType | Returns or sets the turn type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetParent | Set parent |
SetProbeAngles | Set default values for probe angles based on feature type. |
SetProbeTip | Set default probe tip based on preferred tip type and probe angles. |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ApproachDist¶
-
InspectionScanHelixBuilder.
ApproachDist
¶ Returns the builder for approach distance
-------------------------------------
Getter Method
Signature
ApproachDist()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.2.
License requirements: None.
DepthDistance¶
-
InspectionScanHelixBuilder.
DepthDistance
¶ Returns or sets the depth distance
-------------------------------------
Getter Method
Signature
DepthDistance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthDistance(distance)
Parameters: distance (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DepthMethod¶
-
InspectionScanHelixBuilder.
DepthMethod
¶ Returns or sets the depth method
-------------------------------------
Getter Method
Signature
DepthMethod()
Returns: Return type: NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthMethod(method)
Parameters: method ( NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EndDistance¶
-
InspectionScanHelixBuilder.
EndDistance
¶ Returns the End Distance of the Scan Helix
-------------------------------------
Getter Method
Signature
EndDistance()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
EndPercentage¶
-
InspectionScanHelixBuilder.
EndPercentage
¶ Returns the End Percentage of the Scan Helix
-------------------------------------
Getter Method
Signature
EndPercentage()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
Pitch¶
-
InspectionScanHelixBuilder.
Pitch
¶ Returns the pitch of the Scan Helix
-------------------------------------
Getter Method
Signature
Pitch()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
RetractDist¶
-
InspectionScanHelixBuilder.
RetractDist
¶ Returns the builder for retract distance
-------------------------------------
Getter Method
Signature
RetractDist()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.2.
License requirements: None.
Reversedirection¶
-
InspectionScanHelixBuilder.
Reversedirection
¶ Returns or sets the Reverse Direction flag on the Helix
-------------------------------------
Getter Method
Signature
Reversedirection()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Reversedirection(reversedir)
Parameters: reversedir (bool) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Revolutions¶
-
InspectionScanHelixBuilder.
Revolutions
¶ Returns the revolutions of the Scan Helix
-------------------------------------
Getter Method
Signature
Revolutions()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
ScanModeType¶
-
InspectionScanHelixBuilder.
ScanModeType
¶ Returns or sets the 3,5 axis mode type
-------------------------------------
Getter Method
Signature
ScanModeType()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderScanModeTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScanModeType(modeType)
Parameters: modeType ( NXOpen.CAM.InspectionMethodBuilderScanModeTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ScanSpeed¶
-
InspectionScanHelixBuilder.
ScanSpeed
¶ Returns the builder for scan speed
-------------------------------------
Getter Method
Signature
ScanSpeed()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX11.0.0.
License requirements: None.
StartDistance¶
-
InspectionScanHelixBuilder.
StartDistance
¶ Returns the Start Distance of the Scan Helix
-------------------------------------
Getter Method
Signature
StartDistance()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
StartEndMode¶
-
InspectionScanHelixBuilder.
StartEndMode
¶ Returns or sets the start/end mode
-------------------------------------
Getter Method
Signature
StartEndMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartEndMode(startEndMode)
Parameters: startEndMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartPercentage¶
-
InspectionScanHelixBuilder.
StartPercentage
¶ Returns the Start Percentage of the Scan Helix
-------------------------------------
Getter Method
Signature
StartPercentage()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
StepSize¶
-
InspectionScanHelixBuilder.
StepSize
¶ Returns the builder for step size
-------------------------------------
Getter Method
Signature
StepSize()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX11.0.0.
License requirements: None.
Sweep¶
-
InspectionScanHelixBuilder.
Sweep
¶ Returns the sweep of the Scan Helix
-------------------------------------
Getter Method
Signature
Sweep()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
TurnDirection¶
-
InspectionScanHelixBuilder.
TurnDirection
¶ Returns or sets the turn direction type
-------------------------------------
Getter Method
Signature
TurnDirection()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderScanHelixTurnDirectionTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TurnDirection(turnDirection)
Parameters: turnDirection ( NXOpen.CAM.InspectionMethodBuilderScanHelixTurnDirectionTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TurnType¶
-
InspectionScanHelixBuilder.
TurnType
¶ Returns or sets the turn type
-------------------------------------
Getter Method
Signature
TurnType()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderScanHelixTurnTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TurnType(turnType)
Parameters: turnType ( NXOpen.CAM.InspectionMethodBuilderScanHelixTurnTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
InspectionScanHelixBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.