InspectionMoveBuilderDepthMethodTypes Enumeration

NXOpen.CAM.InspectionMoveBuilder.DepthMethodTypes is an alias for NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes

class NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes

Bases: object

the depth method

Enum Members

Enum Member Enum Member Description
Auto
Auto specify
Distance
Distance only
FromFeatureNominal
Distance from feature nominal
FromFeatureActual
Distance from feature actual
FromDatum
Distance from datum
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.