CylinderMillingBuilder Class¶
-
class
NXOpen.CAM.
CylinderMillingBuilder
¶ Bases:
NXOpen.CAM.CylindricalMillingBuilder
Represents a CylinderMillingBuilder Builder
To create a new instance of this class, use
NXOpen.CAM.OperationCollection.CreateCylinderMillingBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AxialDistance | Returns the distance builder for Depth per Revolution |
AxialStepover | Returns the Axial Stepover builder |
BlankDiameter | Returns or sets the start location |
BlankDistance | Returns the Wall Thickness |
ChannelName | Returns or sets the channel’s name |
CleanupPasses | Returns or sets the Cleanup Passes |
CollisionCheck | Returns or sets the collision check for cutting |
CutParameters | Returns the Cylinder Milling Cut Parameters |
CutPattern | Returns or sets the cut pattern |
CuttingParameters | Returns the Cut Parameters |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
DepthPerRevolution | Returns or sets the Depth per Revolution |
Description | Returns or sets the description |
DiameterForHelix | Returns or sets the Diameter for Helix |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
FeedsBuilder | Returns the feeds and speeds builder |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HelixDiameter | Returns the Helix Diamter |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MinimumHelixDiameter | Returns the Minimum Helix Diameter |
MotionOutputBuilder | Returns the motion output builder |
NonCuttingBuilder | Returns the non-cutting moves builder |
Notes | Returns the notes builder |
OffsetFromStartDiameter | Returns the Offset from Start Diameter |
OppositeDirection | Returns or sets the opposite direction |
OppositeDirectionBuilder | Returns the opposite direction builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
RadialStepover | Returns the Radial Stepover builder |
RampAngle | Returns the Ramp Angle |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
SpiralThickness | Returns the Spiral Thickness |
StartDiameter | Returns the Start Diameter |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeatureGeometry | Returns the feature geometry @return |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CylinderMillingBuilderBlankDiameterTypes Enumeration | blank diamter options |
CylinderMillingBuilderCutPatternTypes Enumeration | cut pattern options |
CylinderMillingBuilderDepthPerRevolutionTypes Enumeration | Depth Per Revolution options |
CylinderMillingBuilderDiameterForHelixTypes Enumeration | Diameter for Helix |
Property Detail¶
AxialDistance¶
-
CylinderMillingBuilder.
AxialDistance
¶ Returns the distance builder for Depth per Revolution
-------------------------------------
Getter Method
Signature
AxialDistance()
Returns: the distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
BlankDiameter¶
-
CylinderMillingBuilder.
BlankDiameter
¶ Returns or sets the start location
-------------------------------------
Getter Method
Signature
BlankDiameter()
Returns: the start location type Return type: NXOpen.CAM.CylinderMillingBuilderBlankDiameterTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankDiameter(newValue)
Parameters: newValue ( NXOpen.CAM.CylinderMillingBuilderBlankDiameterTypes
) – the start location typeNew in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
BlankDistance¶
-
CylinderMillingBuilder.
BlankDistance
¶ Returns the Wall Thickness
-------------------------------------
Getter Method
Signature
BlankDistance()
Returns: the wall thickness builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
CleanupPasses¶
-
CylinderMillingBuilder.
CleanupPasses
¶ Returns or sets the Cleanup Passes
-------------------------------------
Getter Method
Signature
CleanupPasses()
Returns: the Cleanup Passes Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CleanupPasses(newValue)
Parameters: newValue (bool) – the Cleanup Passes New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
CutParameters¶
-
CylinderMillingBuilder.
CutParameters
¶ Returns the Cylinder Milling Cut Parameters
-------------------------------------
Getter Method
Signature
CutParameters()
Returns: the Cut Parameters Return type: NXOpen.CAM.CylinderMillingCutParameters
New in version NX8.0.0.
Deprecated since version NX9.0.3: Use
CAM.HoleMachiningBuilder.CuttingParameters()
instead.License requirements: None.
CutPattern¶
-
CylinderMillingBuilder.
CutPattern
¶ Returns or sets the cut pattern
-------------------------------------
Getter Method
Signature
CutPattern()
Returns: the cut pattern type Return type: NXOpen.CAM.CylinderMillingBuilderCutPatternTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutPattern(newValue)
Parameters: newValue ( NXOpen.CAM.CylinderMillingBuilderCutPatternTypes
) – the cut pattern typeNew in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
DepthPerRevolution¶
-
CylinderMillingBuilder.
DepthPerRevolution
¶ Returns or sets the Depth per Revolution
-------------------------------------
Getter Method
Signature
DepthPerRevolution()
Returns: the Depth per Revolution type Return type: NXOpen.CAM.CylinderMillingBuilderDepthPerRevolutionTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthPerRevolution(newValue)
Parameters: newValue ( NXOpen.CAM.CylinderMillingBuilderDepthPerRevolutionTypes
) – the Depth per Revolution typeNew in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
DiameterForHelix¶
-
CylinderMillingBuilder.
DiameterForHelix
¶ Returns or sets the Diameter for Helix
-------------------------------------
Getter Method
Signature
DiameterForHelix()
Returns: the Diameter for Helix type Return type: NXOpen.CAM.CylinderMillingBuilderDiameterForHelixTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiameterForHelix(newValue)
Parameters: newValue ( NXOpen.CAM.CylinderMillingBuilderDiameterForHelixTypes
) – the Diameter for Helix typeNew in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
HelixDiameter¶
-
CylinderMillingBuilder.
HelixDiameter
¶ Returns the Helix Diamter
-------------------------------------
Getter Method
Signature
HelixDiameter()
Returns: the diamter Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
MinimumHelixDiameter¶
-
CylinderMillingBuilder.
MinimumHelixDiameter
¶ Returns the Minimum Helix Diameter
-------------------------------------
Getter Method
Signature
MinimumHelixDiameter()
Returns: the minimum helix diameter builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
OffsetFromStartDiameter¶
-
CylinderMillingBuilder.
OffsetFromStartDiameter
¶ Returns the Offset from Start Diameter
-------------------------------------
Getter Method
Signature
OffsetFromStartDiameter()
Returns: the offset from start diamter builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX9.0.0.
License requirements: None.
OppositeDirection¶
-
CylinderMillingBuilder.
OppositeDirection
¶ Returns or sets the opposite direction
-------------------------------------
Getter Method
Signature
OppositeDirection()
Returns: the opposite direction Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OppositeDirection(newValue)
Parameters: newValue (bool) – the opposite direction New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
OppositeDirectionBuilder¶
-
CylinderMillingBuilder.
OppositeDirectionBuilder
¶ Returns the opposite direction builder
-------------------------------------
Getter Method
Signature
OppositeDirectionBuilder()
Returns: the opposite direction builder Return type: NXOpen.CAM.OppositeDirection
New in version NX8.5.0.
Deprecated since version NX9.0.0: Change the Z-axis of the in-process feature instead.
License requirements: None.
RampAngle¶
-
CylinderMillingBuilder.
RampAngle
¶ Returns the Ramp Angle
-------------------------------------
Getter Method
Signature
RampAngle()
Returns: the Ramp Angle builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.0.0.
License requirements: None.
SpiralThickness¶
-
CylinderMillingBuilder.
SpiralThickness
¶ Returns the Spiral Thickness
-------------------------------------
Getter Method
Signature
SpiralThickness()
Returns: the spiral thickness builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
StartDiameter¶
-
CylinderMillingBuilder.
StartDiameter
¶ Returns the Start Diameter
-------------------------------------
Getter Method
Signature
StartDiameter()
Returns: the start diamter builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CylinderMillingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.