CylinderMillingCutParameters Class¶
-
class
NXOpen.CAM.
CylinderMillingCutParameters
¶ Bases:
NXOpen.CAM.CylindricalMillingCutParameters
Represents a CylinderMillingCutParameters Builder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
BottomOffset | Returns the bottom offset |
BottomStock | Returns the bottom stock |
CheckIpwCollisions | Returns or sets the value to Check for Ipw Collsions |
CheckSafeClearance | Returns the Check Safe Clearance |
ContinuousCut | Returns or sets the continuous cut |
CutDirection | Returns or sets the cut direction |
CuttingDirection | Returns or sets the cut direction |
HolderClearance | Returns the Holder Clearance |
IpwType | Returns or sets the IPW type |
NeckClearance | Returns the Neck Clearance |
PartSafeClearance | Returns the Part Safe Clearance |
PartStock | Returns the part stock |
ShankClearance | Returns the Shank Clearance |
Tag | Returns the Tag for this object. |
Tolerances | Returns the Tolerances builder |
TopOffset | Returns the top offset |
UseToolHolder | Returns or sets the use tool holder |
Methods¶
Enumerations¶
CylinderMillingCutParametersCutDirectionTypes Enumeration | cut direction options |
Property Detail¶
CutDirection¶
-
CylinderMillingCutParameters.
CutDirection
¶ Returns or sets the cut direction
-------------------------------------
Getter Method
Signature
CutDirection()
Returns: the cut directon type Return type: NXOpen.CAM.CylinderMillingCutParametersCutDirectionTypes
New in version NX8.0.0.
Deprecated since version NX9.0.2: Use
NXOpen.CAM.FeatureMillingCutParameters.CuttingDirection`()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
CutDirection(cutDir)
Parameters: cutDir ( NXOpen.CAM.CylinderMillingCutParametersCutDirectionTypes
) – the cut directon typeNew in version NX8.0.0.
Deprecated since version NX9.0.2: Use
NXOpen.CAM.FeatureMillingCutParameters.CuttingDirection`()
instead.License requirements: cam_base (“CAM BASE”)